2010-09-13 23:50:35     no "images" directory created

Document created by Aaronwu Employee on Aug 22, 2013
Version 1Show Document
  • View in full screen mode

2010-09-13 23:50:35     no "images" directory created

alex litz (UNITED STATES)

Message: 93393   

 

Hey all,

 

After installing the toolchain twice, making certain that the uClinux distributation matches, etc..., I'm having some issues compiling.

 

"make" yields an error near the end:

 

make[3]: Leaving directory `/home/alitz/ucLinux/uClinux-dist/user/play'

bfin-uclinux-gcc  -Wl,-elf2flt    -mcpu=bf526-0.0  pmap_dump.o   -o pmap_dump

bfin-uclinux-gcc  -Wl,-elf2flt    -mcpu=bf526-0.0  pmap_set.o   -o pmap_set

  GEN     /home/alitz/ucLinux/uClinux-dist/user/busybox/build-busybox-1.13.4/Makefile

  Using /home/alitz/ucLinux/uClinux-dist/user/busybox/busybox-1.13.4 as source for busybox

make[4]: Leaving directory `/home/alitz/ucLinux/uClinux-dist/user/portmap/portmap_6.0'

make[3]: Leaving directory `/home/alitz/ucLinux/uClinux-dist/user/portmap'

make[4]: Leaving directory `/home/alitz/ucLinux/uClinux-dist/user/busybox/build-busybox-1.13.4'

make[3]: Leaving directory `/home/alitz/ucLinux/uClinux-dist/user/busybox'

make[2]: Leaving directory `/home/alitz/ucLinux/uClinux-dist/user'

make[1]: *** [all] Error 2

make[1]: Leaving directory `/home/alitz/ucLinux/uClinux-dist/user'

make: *** [subdirs] Error 1

 

 

Its creating the "linux" and "vmlinux" elf files under the linux.2.6.xx directory, but not creating the image files...doing a manual make image is also not yielding the desired results.

 

Any clues?

 

 

 

Cheers,

QuoteReplyEditDelete

 

 

2010-09-14 00:02:08     Re: no "images" directory created

Mike Frysinger (UNITED STATES)

Message: 93394   

 

you didnt post enough of a log.  you need to look up to figure out what the actual problem is.

 

or run `make single` so that the build aborts on an error.

QuoteReplyEditDelete

 

 

2010-09-14 00:27:02     Re: no "images" directory created

alex litz (UNITED STATES)

Message: 93395   

 

Thanks Mike - I figured it out, apparently I didn't find the instructions on setting up the host system, though Im a bit confused on why I would need host header files to compile the target correctly - seems dangerous.

 

I am now able to compile, but it crashes when I load uImage into u-boot, and try to "go"....I will see if I can sift through the documentation on what I am doing wrong now.

 

 

 

Thanks,

QuoteReplyEditDelete

 

 

2010-09-14 00:36:02     Re: no "images" directory created

Mike Frysinger (UNITED STATES)

Message: 93397   

 

you dont use 'go' on any file in images/.  you use 'bootm' on uimages.

QuoteReplyEditDelete

 

 

2010-09-14 00:40:31     Re: no "images" directory created

alex litz (UNITED STATES)

Message: 93398   

 

Thanks Mike, just figured that out as well....I gotta say, its neat to have this thing up and running...looking forward to porting it to our custom board

 

I am just wondering at this point, and I may start a topic on this, how does one deal with source control with all the third party-dependencies on the host system?   Do you have to image the entire system, or is there documentation on how to pull out the dependencies...

 

Cheers,

 

Alex

QuoteReplyEditDelete

 

 

2010-09-14 00:45:04     Re: no "images" directory created

Mike Frysinger (UNITED STATES)

Message: 93399   

 

new thread please

Attachments

    Outcomes