2010-09-03 07:59:20     Adding eth1network interface

Document created by Aaronwu Employee on Aug 22, 2013
Version 1Show Document
  • View in full screen mode

2010-09-03 07:59:20     Adding eth1network interface

JAYAKAR Nalthooru (INDIA)

Message: 93106   

 

Dear All,

 

I am new to uClinux system. My hardware supports two Ethernet interfaces. Interface eth0 is up and running. I want to add eth1 interface. Both eth0 & eth1 hardware are same. Can you please suggest me how to add the same to network driver interface.

 

Thanks in advance,

 

Jay

QuoteReplyEditDelete

 

 

2010-09-03 11:19:22     Re: Adding eth1network interface

Mike Frysinger (UNITED STATES)

Message: 93113   

 

your description is too vague as to what the problem is.  if the devices are the same, then declare them the same (however it is you did that).

 

otherwise, you'll need to describe what is wrong -- does `ifconfig eth1` not work ?

Attachments

    Outcomes