2010-07-22 15:19:51     Using the serial gadget driver with Windows 7 64 bit

Document created by Aaronwu Employee on Aug 22, 2013
Version 1Show Document
  • View in full screen mode

2010-07-22 15:19:51     Using the serial gadget driver with Windows 7 64 bit

Adam Rosenberg (UNITED STATES)

Message: 91611   

 

I was able to get Windows 7 64 bit to connect with the Net2272 chip on my BF537 based custom board but had to update the Windows .inf file using instructions I found here:

  blogs.6bit.com/josh/2009/10/usb-communications-device-class-on-64-bit-windows/

 

It would be nice to link to that page from this slightly out-dated page that got me close...

  docs.blackfin.uclinux.org/doku.php?id=linux-kernel:usb-gadget:serial

 

Thanks,

Adam

QuoteReplyEditDelete

 

 

2010-07-22 15:56:54     Re: Using the serial gadget driver with Windows 7 64 bit

Robin Getz (UNITED STATES)

Message: 91612   

 

Adam:

 

As long as you agree to the terms and conditions that are in:

 

https://docs.blackfin.uclinux.org/doku.php?id=copyright_information#contributing_to_this_document

 

I can add you to the docs committers list, and you can add/edit yourself.

 

-Robin

QuoteReplyEditDelete

 

 

2010-07-22 16:14:35     Re: Using the serial gadget driver with Windows 7 64 bit

Adam Rosenberg (UNITED STATES)

Message: 91613   

 

Robin,

 

I can agree to those terms and do not mind editting the page, but is there some kind of review system in place?  I don't want to change a document and have it take effect immediately (just in case someone doesn't like the change).

 

Thanks,

Adam

QuoteReplyEditDelete

 

 

2010-07-22 17:11:01     Re: Using the serial gadget driver with Windows 7 64 bit

Mike Frysinger (UNITED STATES)

Message: 91616   

 

all changes are sent out to a mailing list where anyone can monitor.  all the devs are on it.

QuoteReplyEditDelete

 

 

2010-07-22 18:03:13     Re: Using the serial gadget driver with Windows 7 64 bit

Robin Getz (UNITED STATES)

Message: 91618   

 

Adam:

 

You should be set -- like Mike said - if we don't like something - we change it back pretty quickly - there is revision control in the wiki

 

-Robin

QuoteReplyEditDelete

 

 

2010-07-22 21:18:57     Re: Using the serial gadget driver with Windows 764 bit

Adam Rosenberg (UNITED STATES)

Message: 91629    Robin,

 

Thanks, I just modified the page and it was pretty quick and easy.

 

This is off topic, but once I get some DMA buffer problem fixed with

my CS42448 ALSA driver (I have some clicking sounds when playing), I'd

like to help add some information to the alsa page

(https://docs.blackfin.uclinux.org/doku.php?id=linux-kernel:alsa) as

well. Is there someone who I should collaborate on this with or just

add it and let people see?

 

Thanks,

Adam

QuoteReplyEditDelete

 

 

2010-07-22 22:05:56     Re: Using the serial gadget driver with Windows 764 bit

Mike Frysinger (UNITED STATES)

Message: 91630   

 

just add it

Attachments

    Outcomes