2010-07-15 02:30:26     ISP1362 with BF532 issues

Document created by Aaronwu Employee on Aug 22, 2013
Version 1Show Document
  • View in full screen mode

2010-07-15 02:30:26     ISP1362 with BF532 issues

Usama Shakeel (PAKISTAN)

Message: 91267   

 

Hello,

 

I am curently working on IP08 board made by Rowetel and it has BF532 and ISP1362 controller for USB. The Problem I am facing is that I am able to use normal USB Mass storage devices they are detected by the system  (uClinux 2009 dist). But when I try to attach MP3 Player or Nokia Phone it does not even show symptoms of being attached to usb port. Although I have compiled ISP1362-HCD and enabled the cdc-acm support as well. Kindly guide me whether it is feasible or not, If yes then where the problem is.. For Reference I am Pasting the Boot Message of uClinux...

 

 

 

Kindly Explain ...

 

## Booting image at 01000000 ...                                              

   Image Name:   Linux Kernel and ext2                                        

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)                

   Data Size:    3975513 Bytes =  3.8 MB                                      

   Load Address: 00001000                                                     

   Entry Point:  00248c9c                                                     

   Verifying Checksum ... OK                                                  

   Uncompressing Kernel Image ... OK                                          

Starting Kernel at = 248c9c                                                   

console [ttyBF0] enabled, bootconsole disabled                                

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)                 

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)                  

Memory available: 53320k/65536k RAM, (128k init code, 1565k kernel code, 735k d)

Calibrating delay loop... 778.24 BogoMIPS (lpj=1556480)                       

Security Framework initialized                                                

Mount-cache hash table entries: 512                                           

Blackfin Scratchpad data SRAM: 4 KB                                           

Blackfin L1 Data A SRAM: 16 KB (16 KB free)                                   

Blackfin L1 Data B SRAM: 16 KB (16 KB free)                                   

Blackfin L1 Instruction SRAM: 48 KB (35 KB free)                              

net_namespace: 424 bytes                                                      

NET: Registered protocol family 16                                            

Blackfin DMA Controller                                                       

ip0x_init(): chip_id=527A50CB,dspid=E5040005                                  

ip0x_init(): registering device resources                                     

SCSI subsystem initialized                                                    

usbcore: registered new interface driver usbfs                                

usbcore: registered new interface driver hub                                  

usbcore: registered new device driver usb                                     

NET: Registered protocol family 2                                             

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)                

TCP established hash table entries: 2048 (order: 2, 16384 bytes)              

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)                      

TCP: Hash tables configured (established 2048 bind 2048)                      

TCP reno registered                                                           

NET: Registered protocol family 1                                             

yaffs Jul 13 2010 13:09:14 Installing.                                        

msgmni has been set to 104                                                    

alg: No test for stdrng (krng)                                                

io scheduler noop registered                                                  

io scheduler anticipatory registered (default)                                

io scheduler cfq registered                                                   

bfin-jtag-comm: initialized                                                   

bfin-dma: initialized                                                         

Serial: Blackfin serial driver                                                

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 21) is a BFIN-UART              

brd: module loaded                                                            

dm9000 Ethernet Driver, V1.31                                                 

eth0: dm9000a at 20100000,20100002 IRQ 48 MAC: 00:19:d1:1f:ff:66 (platform data)

eth1: dm9000a at 20200000,20200002 IRQ 47 MAC: 00:14:bf:6e:20:b6 (platform data)

usbcore: registered new interface driver catc                                 

catc: v2.8:CATC EL1210A NetMate USB Ethernet driver                           

usbcore: registered new interface driver kaweth                               

pegasus: v0.6.14 (2006/09/27), Pegasus/Pegasus II USB Ethernet driver         

usbcore: registered new interface driver pegasus                              

rtl8150: v0.6.2 (2004/08/27):rtl8150 based usb-ethernet driver                

usbcore: registered new interface driver rtl8150                              

usbcore: registered new interface driver asix                                 

usbcore: registered new interface driver cdc_ether                            

usbcore: registered new interface driver net1080                              

usbcore: registered new interface driver cdc_subset                           

usbcore: registered new interface driver zaurus                               

Driver 'sd' needs updating - please use bus_type methods                      

Driver 'sr' needs updating - please use bus_type methods                      

uclinux[mtd]: RAM probe address=0x3700000 size=0x800000                       

Creating 1 MTD partitions on "RAM":                                           

0x00000000-0x00800000 : "ROMfs"                                               

Generic platform RAM MTD, (c) 2004 Simtec Electronics                         

NAND device: Manufacturer ID: 0xec, Chip ID: 0xda (Samsung NAND 256MiB 3,3V 8-b)

Scanning device for bad blocks                                                

Creating 2 MTD partitions on "NAND 256MiB 3,3V 8-bit":                        

0x00000000-0x00800000 : "linux kernel"                                        

0x00800000-0x10000000 : "file system"                                         

aoe: AoE v47 initialised.                                                     

driver isp1362-hcd, 2005-04-04                                                

isp1362-hcd isp1362-hcd.0: ISP1362 Host Controller                            

isp1362-hcd isp1362-hcd.0: new USB bus registered, assigned bus number 1      

isp1362-hcd isp1362-hcd.0: irq 44, io mem 0x20300000                          

isp1362_hc_start:                                                             

isp1362-hcd isp1362-hcd.0: ISP1362 Memory usage:                              

isp1362-hcd isp1362-hcd.0:   ISTL:    2 *  256:      512 @ $0000:$0100        

isp1362-hcd isp1362-hcd.0:   INTL:   16 * ( 64+8):  1152 @ $0200              

isp1362-hcd isp1362-hcd.0:   ATL :   32 * ( 64+8):  2304 @ $0680              

isp1362-hcd isp1362-hcd.0:   USED/FREE:   3968       128                      

usb usb1: configuration #1 chosen from 1 choice                               

hub 1-0:1.0: USB hub found                                                    

hub 1-0:1.0: 2 ports detected                                                 

usb usb1: New USB device found, idVendor=1d6b, idProduct=0001                 

usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1            

usb usb1: Product: ISP1362 Host Controller                                    

usb usb1: Manufacturer: Linux 2.6.28.10-ADI-2009R1.1 isp1362-hcd              

usb usb1: SerialNumber: isp1362-hcd.0                                         

ISP1362 Host Controller, irq 44                                               

usbcore: registered new interface driver cdc_acm                              

cdc_acm: v0.26:USB Abstract Control Model driver for USB modems and ISDN adaptes

Initializing USB Mass Storage driver...                                       

usbcore: registered new interface driver usb-storage                          

USB Mass Storage support registered.                                          

usbcore: registered new interface driver ati_remote                           

ati_remote: 2.2.1:ATI/X10 RF USB Remote Control                               

usbcore: registered new interface driver ati_remote2                          

ati_remote2: ATI/Philips USB RF remote driver 0.3                             

usbcore: registered new interface driver keyspan_remote                       

usbcore: registered new interface driver yealink                              

yealink: yld-20051230:Yealink phone driver                                    

cm109: Keymap for Komunikate KIP1000 phone loaded                             

usbcore: registered new interface driver cm109                                

cm109: CM109 phone driver: 20080805 (C) Alfred E. Heggestad                   

bfin-wdt: initialized: timeout=20 sec (nowayout=0)                            

Linux telephony interface: v1.00                                              

IPVS: Registered protocols ()                                                 

IPVS: Connection hash table configured (size=4096, memory=32Kbytes)           

IPVS: ipvs loaded.                                                            

ip_tables: (C) 2000-2006 Netfilter Core Team                                  

TCP cubic registered                                                          

NET: Registered protocol family 17                                            

NET: Registered protocol family 35                                            

yaffs: dev is 32505858 name is "mtdblock2"                                    

yaffs: passed flags ""                                                        

yaffs: Attempting MTD mount on 31.2, "mtdblock2"                              

yaffs: auto selecting yaffs2                                                  

Partially written block 748 detected                                          

Partially written block 748 detected                                          

yaffs_read_super: isCheckpointed 0

VFS: Mounted root (yaffs filesystem).

Freeing unused kernel memory: 128k freed

dma_alloc_init: dma_page @ 0x0025c000 - 256 pages at 0x03f00000

eth0: link down

eth0: link up, 100Mbps, full-duplex, lpa 0x45E1

/proc/sys/vm/pagecache_ratio: cannot create

modprobe: cannot parse modules.dep

Failed to open /dev/zap/ctl: No such device or address

Notice: Configuration file is /etc/zaptel.conf

line 0: Unable to open master device '/dev/zap/ctl'

 

1 error(s) detected

 

 

Welcome to:

       ____ _  _

      /  __| ||_|             _  _

_   _| |  | | _ ____  _   _ \ \/ /

| | | | |  | || |  _ \| | | | \  /

| |_| | |__| || | | | | |_| | /  \

|  ___\____|_||_|_| |_|\____|/_/\_\

|_| IP04/IP08 Open Hardware IP-PBX

 

Blackfin Asterisk Build System (BAPS) Edition

 

For further information see:

    www.rowetel.com/ucasterisk/ip04.html

    www.rowetel.com/ucasterisk/baps.html

 

Thanks to the BAPS, Astfin, BlackfinOne, and Asterisk communities;

Analog Devices and Atcom.

 

 

BusyBox v1.4.1 (2008-10-31 16:21:50 PKT) Built-in shell (msh)

Enter 'help' for a list of built-in commands.

 

==>> yaffs bug: fs/yaffs2/yaffs_guts.c 6832

==>> yaffs bug: fs/yaffs2/yaffs_guts.c 6759

==>> yaffs bug: fs/yaffs2/yaffs_guts.c 6759

root:~> ==>> yaffs bug: fs/yaffs2/yaffs_guts.c 6832

==>> yaffs bug: fs/yaffs2/yaffs_guts.c 6759

==>> yaffs bug: fs/yaffs2/yaffs_guts.c 6759

Attachments

    Outcomes