2010-07-01 09:47:06     BF561 and Ethernet

Document created by Aaronwu Employee on Aug 22, 2013
Version 1Show Document
  • View in full screen mode

2010-07-01 09:47:06     BF561 and Ethernet

blue hash (UNITED STATES)

Message: 90806   

 

Hello,

 

I'm familiar with loading u-boot and uClinux over ethernet on the BF537 stamp kit. However how is this done on the BF561 kit? Does it use the EZ-LAN extender kit? This link has everything to get me started, but I was wondering if it is supported in the latest uClinux and uBoot builds.

 

Thanks!

QuoteReplyEditDelete

 

 

2010-07-01 10:05:35     Re: BF561 and Ethernet

Stephen Lombard (AUSTRALIA)

Message: 90807   

 

Hey,

 

I use the BF561-EZKIT with the EZ-LAN extender.  It has a SMSC91111 chip on it which is well supported in U-Boot and uClinux as well.

 

Just note that when you do get the EZ-LAN extender there's a bank of two switches which you'll have to adjust as per the page on this site somewhere.  Mine came with the switches already set correctly but that was 2 years ago, so just check yours.

 

Regards,

 

Stephen Lombard

QuoteReplyEditDelete

 

 

2010-07-01 11:51:04     Re: BF561 and Ethernet

blue hash (UNITED STATES)

Message: 90810   

 

Thanks Stephen!

Attachments

    Outcomes