2010-06-24 16:55:03     BF527 LCD driver

Document created by Aaronwu Employee on Aug 22, 2013
Version 1Show Document
  • View in full screen mode

2010-06-24 16:55:03     BF527 LCD driver

Phil Burkert (UNITED STATES)

Message: 90609   

 

Hi,

 

The documentation wiki link is not working today. Does the latest kernel include support for the BF527 EZ-KIT LCD touch panel?

 

Thanks,

 

Phil

QuoteReplyEditDelete

 

 

2010-06-24 17:03:03     Re: BF527 LCD driver

Phil Burkert (UNITED STATES)

Message: 90610   

 

I just read Hans' thread which indicates no driver for the BF527 EZ-KIT LCD panel. I can monitor that thread for further updates. Thanks. -Phil

QuoteReplyEditDelete

 

 

2010-06-24 21:22:03     Re: BF527 LCD driver

Mike Frysinger (UNITED STATES)

Message: 90617   

 

the last release works fine with the BF527-EZKIT LCD

QuoteReplyEditDelete

 

 

2010-06-25 03:25:54     Re: BF527 LCD driver

Michael Hennerich (GERMANY)

Message: 90637    There are LCD/TFT framebuffer drivers for all versions of BF527-EZKITs.

 

RGB888 (24-bit RGB) support for EZKIT Rev. < 2.1

And

RGB565 (16-bit RGB) and RGB888 for EZKIT Rev. >= 2.1

Later one also includes a AD7879 Touch screen digitizer + ADP5520 Keypad controller.

For all those peripherals are Linux drivers available.

 

-Michael

Attachments

    Outcomes