2010-06-09 08:27:28     Error while trying to excute Hello World on STAMP

Document created by Aaronwu Employee on Aug 22, 2013
Version 1Show Document
  • View in full screen mode

2010-06-09 08:27:28     Error while trying to excute Hello World on STAMP

Jithender Golamari (IRELAND)

Message: 90222   

 

Hi There, I followed

 

  docs.blackfin.uclinux.org/doku.php?id=simple_hello_world_application_example&s[]=hello&s[]=world

 

for compiling a hello world program and FTP the file to BF533 in binary.

 

but after running chmod 777 hello and tried to execute the file with the command ./hello on STAMP

 

I got the following error message.

 

/helloBINFMT_FLAT: bad magic/rev (0x4, need 0x5)

BINFMT_FLAT:

bad magic/rev (0x4, need 0x5)

hello: applet not found

 

 

 

I had also went through   docs.blackfin.uclinux.org/doku.php?id=faq

 

but with no luck as the answer for that error was to use the command

 

bfin-uclinux-gcc -Wl,-elf2flt hello.c -o hello

 

which I already did.

 

Can some1 help please???

 

Thank you

 

 

 

 

 

QuoteReplyEditDelete

 

 

2010-06-09 09:11:44     Re: Error while trying to excute Hello World on STAMP

Robin Getz (UNITED STATES)

Message: 90223   

 

Jithender:

 

You are using a kernel which is too old - upgrade to something more recent.

 

-Robin

QuoteReplyEditDelete

 

 

2010-06-09 09:21:24     Re: Error while trying to excute Hello World on STAMP

Jithender Golamari (IRELAND)

Message: 90224   

 

cool, thnkx a million, will try that

 

 

QuoteReplyEditDelete

 

 

2010-06-10 06:35:53     Re: Error while trying to excute Hello World on STAMP

Jithender Golamari (IRELAND)

Message: 90246   

 

Hi Robin,

 

Tried to update kernel on BF533 but with no luck, so I tried to use the 2006 toolchain as the STAMP I have has the kernel of 2005 but that didnt help either. Can you please advise me on this any weblinks or anything at all. Thank you.

 

Jithender

QuoteReplyEditDelete

 

 

2010-06-10 10:44:41     Re: Error while trying to excute Hello World on STAMP

Robin Getz (UNITED STATES)

Message: 90247   

 

Jithender:

 

The only option is to upgrade everything.

 

What did you have problems with?

 

-Robin

QuoteReplyEditDelete

 

 

2010-06-11 05:28:41     Re: Error while trying to excute Hello World on STAMP

Jithender Golamari (IRELAND)

Message: 90263   

 

Robin,

 

I am not sure in-regards of  upgrading kernel on BF533, can you help me with this please.

 

Thank you

 

 

 

Jithender

QuoteReplyEditDelete

 

 

2010-06-11 11:34:31     Re: Error while trying to excute Hello World on STAMP

Robin Getz (UNITED STATES)

Message: 90269   

 

Jithender:

 

 

 

  docs.blackfin.uclinux.org/doku.php?id=bootloaders:u-boot:upgrading

 

  docs.blackfin.uclinux.org/doku.php?id=bootloaders:u-boot:parallel-flash

 

  docs.blackfin.uclinux.org/doku.php?id=bootloaders:u-boot:tftp_loading_files

 

QuoteReplyEditDelete

 

 

2010-06-11 13:41:18     Re: Error while trying to excute Hello World on STAMP

Jithender Golamari (IRELAND)

Message: 90270   

 

Thanks for the link:)

 

Jithender

Attachments

    Outcomes