2010-04-26 22:24:46     Some time write data to server failed using samaba

Document created by Aaronwu Employee on Aug 21, 2013
Version 1Show Document
  • View in full screen mode

2010-04-26 22:24:46     Some time write data to server failed using samaba

Bill Xie (CHINA)

Message: 88920   

 

Hi,

 

   I test samaba client in ADSP-BF518 EZ-Board V0.2 + uClinux-dist-2009R1.1-RC4 .libsmbclient.a is from samba-3.025a.Windows Xp is as server.Using Samclient_test.tar.gz to test can occur many times write data to server failed

 

(many be need some hours).

 

Best Regards

 

 

 

-Bill

 

Sambclient_test.tar.gz

QuoteReplyEditDelete

 

 

2010-04-27 00:06:56     Re: Some time write data to server failed using samaba

Mike Frysinger (UNITED STATES)

Message: 88925   

 

so try a newer samba version

QuoteReplyEditDelete

 

 

2010-04-27 02:42:52     Re: Some time write data to server failed using samaba

Bill Xie (CHINA)

Message: 88934   

 

Mike,

 

    Thank you.

 

    I downloaded the lastest version 3.5.2.Using blackfin toolchain compiled,but the libsmbclient.a cann't work with program. I use underside comand to create Makefile and build

 

    ./configure --host=bfin-uclinux --target=bfin-uclinux --build=i686 CC=bfin-uclinux-gcc AR=bfin-uclinux-ar\

         --prefix= --with-smbmount --with-privatedir=/etc/config \

                        --with-configdir=/etc/config --with-logfilebase=/var/log \

                        --without-ldap --disable-cups --disable-pie \

                        --disable-shared --disable-debug --disable-developer \

                        --disable-krb5developer --disable-dmalloc --disable-nls

 

    make

 

 

 

  Is it right to configure Makefile for blackfin uClinux to compile sama-3.5.2?

 

 

-Bill

QuoteReplyEditDelete

 

 

2010-04-27 06:56:40     Re: Some time write data to server failed using samaba

Yi Li (CHINA)

Message: 88959   

 

Bill,

 

> but the libsmbclient.a cann't work with program

 

You need to tell details when you ask for help. Otherwise people don't know how to help you.

 

-Yi

QuoteReplyEditDelete

 

 

2010-05-19 22:04:54     Re: Some time write data to server failed using samaba

Bill Xie (CHINA)

Message: 89565   

 

     Using samba 3.5.2 version in bf516 0.1, board is as client and pc+windows xp is as server. It not occur writing data failed to server using libsmbclient.a. But when program work a hour, it will be exception.

 

The message:

 

Data access misaligned address violation

- Attempted misaligned data memory or data cache access.

Deferred Exception context

CURRENT PROCESS:

COMM=smb_test_bandwi PID=152

CPU = 0

TEXT = 0x01000040-0x012b8540        DATA = 0x012b8560-0x013e8d1c

BSS = 0x013e8d1c-0x013f7380  USER-STACK = 0x0147cf4c

 

return address: [0x01274cd0]; contents of:

0x01274cb0:  d334  9110  0981  1808  e14a  013e  e10a  d338

0x01274cc0:  9110  0981  1819  e300  19c5  3210  e801  0000

0x01274cd0: [e410] 0011  0010  e14a  013e  e10a  d330  9110

0x01274ce0:  0981  17e4  e14a  013d  e10a  c060  e410  0011

 

ADSP-BF516-0.1 400(MHz CCLK) 80(MHz SCLK) (mpu off)

Linux version 2.6.28.10-ADI-2009R1.1

Built with gcc version 4.1.2 (ADI svn)

 

SEQUENCER STATUS:        Not tainted

SEQSTAT: 00002024  IPEND: 0030  SYSCFG: 0006

  EXCAUSE   : 0x24

  interrupts disabled

  physical IVG5 asserted : <0x00009190> { _evt_ivhw + 0x0 }

RETE: <0x00000000> /* Maybe null pointer? */

RETN: <0x01e96000> /* kernel dynamic memory */

RETX: <0x00000480> /* Maybe fixed code section */

RETS: <0x01282442> [ smb_test_bandwi + 0x282402 ]

PC  : <0x01274cd0> [ smb_test_bandwi + 0x274c90 ]

DCPLB_FAULT_ADDR: <0xc0000058> /* kernel dynamic memory */

ICPLB_FAULT_ADDR: <0x01274cd0> [ smb_test_bandwi + 0x274c90 ]

 

PROCESSOR STATE:

R0 : c0000016    R1 : c0000016    R2 : 019af86b    R3 : 019b082c

R4 : 019b1118    R5 : 019afa84    R6 : 00000830    R7 : fffffffe

P0 : 0000006b    P1 : 0000036a    P2 : c0000016    P3 : 019b082c

P4 : 013dc054    P5 : 013dc054    FP : 019af8d8    SP : 01e95f24

LB0: 01288031    LT0: 01288030    LC0: 00000000

LB1: 01286d9d    LT1: 01286d9c    LC1: 00000000

B0 : 8000746e    L0 : 00000000    M0 : 000007e0    I0 : 0147cfe0

B1 : 8977beb7    L1 : 00000000    M1 : 7bb6169e    I1 : 019b48f8

B2 : 0147bb58    L2 : 00000000    M2 : 8000746e    I2 : 00000007

B3 : 00000000    L3 : 00000000    M3 : 846e0e8f    I3 : 0000001e

A0.w: 00000022   A0.x: 00000000   A1.w: 00000022   A1.x: 00000000

USP : 019af88c  ASTAT: 02001004

 

Hardware Trace:

   0 Target : <0x0000508c> { _trap_c + 0x0 }

     Source : <0x00008bee> { _exception_to_level5 + 0xae } CALL pcrel

   1 Target : <0x00008b40> { _exception_to_level5 + 0x0 }

     Source : <0x000089fc> { _bfin_return_from_exception + 0x18 } RTX

   2 Target : <0x000089e4> { _bfin_return_from_exception + 0x0 }

     Source : <0x00008a98> { _ex_trap_c + 0x6c } JUMP.S

   3 Target : <0x00008a2c> { _ex_trap_c + 0x0 }

     Source : <0x00008cba> { _trap + 0x5a } JUMP (P4)

   4 Target : <0x00008c60> { _trap + 0x0 }

     Source : <0x01274ccc> [ smb_test_bandwi + 0x274c8c ] 0xe801

   5 Target : <0x01274cca> [ smb_test_bandwi + 0x274c8a ]

     Source : <0x01278076> [ smb_test_bandwi + 0x278036 ] RTS

   6 Target : <0x01278070> [ smb_test_bandwi + 0x278030 ]

     Source : <0x0127806a> [ smb_test_bandwi + 0x27802a ] IF !CC JUMP

   7 Target : <0x01278061> [ smb_test_bandwi + 0x278021 ]

     Source : <0x0127806e> [ smb_test_bandwi + 0x27802e ] JUMP.S

   8 Target : <0x0127806c> [ smb_test_bandwi + 0x27802c ]

     Source : <0x01278065> [ smb_test_bandwi + 0x278025 ]

   9 Target : <0x01278060> [ smb_test_bandwi + 0x278020 ]

     Source : <0x0000918c> { __common_int_entry + 0xcc } RTI

  10 Target : <0x0000912a> { __common_int_entry + 0x6a }

     Source : <0x00008e40> { _system_call + 0xb8 } RTS

  11 Target : <0x00008e3c> { _system_call + 0xb4 }

     Source : <0x00008e2c> { _system_call + 0xa4 } IF !CC JUMP

  12 Target : <0x00008e26> { _system_call + 0x9e }

     Source : <0x00008e16> { _system_call + 0x8e } IF !CC JUMP

  13 Target : <0x00008df6> { _system_call + 0x6e }

     Source : <0x00008fd4> { _schedule_and_signal_from_int + 0x34 } JUMP.S

  14 Target : <0x00008fd2> { _schedule_and_signal_from_int + 0x32 }

     Source : <0x000016ea> { _finish_atomic_sections + 0x32 } RTS

  15 Target : <0x000016e4> { _finish_atomic_sections + 0x2c }

     Source : <0x000016d4> { _finish_atomic_sections + 0x1c } IF !CC JUMP

Userspace Stack

Stack info:

SP: [0x019af88c] <0x019af88c> /* kernel dynamic memory */

Memory from 0x019af880 to 019b0000

019af880: e3fe601a  019af8d8 <01282442>[019be145] e1050738  6006ae0c  300d3007  daeae3fe

019af8a0: 1be80c00  6100640e  643d0806  63f813f6  01276c66  00100528  05783208  e1200167

019af8c0: e147ff80  914a019b  6e4de107  99516fa6  9b105608  30073049  019afa54 <01271a38>

019af8e0: 013d4ea0  e3ff300f  000047d5  e14a0167  6fa6019b  c9c4e10a  9910b130  10130c00

019af900: 8770e3fe  10070c80  019be140  aef4e100  47c0e3ff  18040c00  e3ff6000  a1300b6f

019af920: ffcce3ff  01276c66  00000010  01670568  6fa64800  30293030  e1401807  e100019b

019af940: e3ff8920  480e44db  6000180a  8832e3fe  e3fe6008  6010882f  882ce3fe  019be140

019af960: 6e43e100  e3fe6011  0c808afb  100d3038  019be140  e1006001  e3ff8920  20044659

019af980: e3fe3007  30388845  00000000  1019481e  e3ff3005  e3feffad  30078c01  e3fe6001

019af9a0: 3007884d  e3fe6009  30078849  e3fe6011  20078845  e3fe3007  481687fd  67ff1804

019af9c0: 13f90d17  01276c66  00100528  60016040  ffaee2ff  e14a05ed  0167019b  cdc8e10a

019af9e0: 30286fa6  303a3031  300e9155  30173005  8dcee3fe  30080c38  60221405  08109128

019afa00: 6c661bf5  01273001  001005ad  0d000167  181e6f86  6461304e  e3ff6002  0c38ffdd

019afa20: a0f21817  007fe120  0c015442  c6821005  434001c2  3001200e  43006408  0d004d08

019afa40: 60001003  e1202006  500103e8  63f82002  01276c86  019b10e4 <01271d7e> 013dc054

019afa60: 013dc054  00000026  00000830  019afa84  0c8086b9  181e3008  14110c00  9110ad72

019afa80: e3ff304a  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afaa0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afac0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afae0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afb00: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afb20: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afb40: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afb60: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afb80: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afba0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afbc0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afbe0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afc00: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afc20: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afc40: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afc60: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afc80: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afca0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afcc0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afce0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afd00: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afd20: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afd40: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afd60: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afd80: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afda0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afdc0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afde0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afe00: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afe20: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afe40: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afe60: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afe80: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afea0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afec0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019afee0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019aff00: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019aff20: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019aff40: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019aff60: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019aff80: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019affa0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019affc0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

019affe0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

Return addresses in stack:

    address : <0x01282442> [ smb_test_bandwi + 0x282402 ]

    address : <0x01271a38> [ smb_test_bandwi + 0x2719f8 ]

    address : <0x01271d7e> [ smb_test_bandwi + 0x271d3e ]

 

 

 

Best regards

 

-Bill

QuoteReplyEditDelete

 

 

2010-05-20 00:14:18     Re: Some time write data to server failed using samaba

Mike Frysinger (UNITED STATES)

Message: 89566   

 

please read the documentation

 

  docs.blackfin.uclinux.org/doku.php?id=uclinux-dist:analyzing_traces#unaligned_data_access

QuoteReplyEditDelete

 

 

2010-05-20 02:34:12     Re: Some time write data to server failed using samaba

Bill Xie (CHINA)

Message: 89572   

 

Mike,

 

    Thank you. I have read this doc. But when according to the way to find the bug.

 

$  bfin-uclinux-addr2line -f -e smb_test_bandwidth.gdb  0x274c90

thread_self

libpthread/linuxthreads.old/internals.h:422

 

So I post this problem for help.

 

Best Regards

 

-Bill

 

QuoteReplyEditDelete

 

 

2010-05-20 03:18:59     Re: Some time write data to server failed using samaba

Mike Frysinger (UNITED STATES)

Message: 89584   

 

build things as FDPIC instead of FLAT to get a better break down.  inlined functions often show up like that.

QuoteReplyEditDelete

 

 

2010-05-20 03:34:38     Re: Some time write data to server failed using samaba

Bill Xie (CHINA)

Message: 89588   

 

Mike,

 

   Thank you. Lib build with bfin-uclinux-,cann't  use bfin-linux-uclibc- to build. Do you know have tools to translate

 

FLAT lib to FDPIC lib?

 

Best Regards

 

-Bill

QuoteReplyEditDelete

 

 

2010-05-20 10:00:55     Re: Some time write data to server failed using samaba

Robin Getz (UNITED STATES)

Message: 89590   

 

Bill:

 

Run make clean, change the build system to fdpic, and build again.

 

-Robin

QuoteReplyEditDelete

 

 

2010-05-20 21:21:43     Re: Some time write data to server failed using samaba

Bill Xie (CHINA)

Message: 89605   

 

Robin,

 

   Thank you for your reply.The samba lib is not in uClinux.

 

Best Regards

 

-Bill

QuoteReplyEditDelete

 

 

2010-05-21 13:15:25     Re: Some time write data to server failed using samaba

Robin Getz (UNITED STATES)

Message: 89642   

 

Bill:

 

All you should need to do is configure things properly with ./configure then.

 

-Robin

QuoteReplyEditDelete

 

 

2010-05-24 04:01:25     Re: Some time write data to server failed using samaba

Bill Xie (CHINA)

Message: 89796   

 

Robin,

 

    Thank you.  In ./configure  using cross compiled with bfin-uclibc-linux- will be occur error.

 

-Bill

 

     

 

QuoteReplyEditDelete

 

 

2010-05-24 11:15:17     Re: Some time write data to server failed using samaba

Robin Getz (UNITED STATES)

Message: 89803   

 

Bill:

 

What error?

QuoteReplyEditDelete

 

 

2010-05-25 02:48:45     Re: Some time write data to server failed using samaba

Bill Xie (CHINA)

Message: 89820   

 

Robin,

 

   Thank you for your reply.It is  my mistake cause to use ./configure failed.

 

Best Regards

 

-Bill

QuoteReplyEditDelete

 

 

2010-05-25 22:52:17     Re: Some time write data to server failed using samaba

Bill Xie (CHINA)

Message: 89850   

 

   Using Fdpic format program work some times with exception.The error message below:

 

 

 

Data access CPLB miss

- Used by the MMU to signal a CPLB miss on a data access.

Deferred Exception context

CURRENT PROCESS:

COMM=smb_test_bandwi PID=174

CPU = 0

TEXT = 0x01400000-0x017eb588        DATA = 0x002c0588-0x002f9628

BSS = 0x002f9628-0x01020000  USER-STACK = 0x0103fea0

 

return address: [0x01014f34]; contents of:

0x01014f10:  67f9  0981  1413  e51a  0038  9110  0981  1806

0x01014f20:  e51a  0028  9110  0981  1815  e3ff  f854  3218

0x01014f30:  e801  0000 [e418] 0011  0010  e51a  003d  9110

0x01014f40:  0981  17ea  e51b  0021  e801  0000  e418  0011

 

ADSP-BF516-0.1 400(MHz CCLK) 80(MHz SCLK) (mpu off)

Linux version 2.6.28.10-ADI-2009R1.1

Built with gcc version 4.1.2 (ADI svn)

 

SEQUENCER STATUS:        Not tainted

SEQSTAT: 00000026  IPEND: 0030  SYSCFG: 0006

  EXCAUSE   : 0x26

  interrupts disabled

  physical IVG5 asserted : <0x00009190> { _evt_ivhw + 0x0 }

RETE: <0x00000000> /* Maybe null pointer? */

RETN: <0x01116000> [ smb_test_bandwi + 0x0 ]

RETX: <0x00000480> /* Maybe fixed code section */

RETS: <0x0114d37e> [ /lib/libc.so.0 + 0xd37e ]

PC  : <0x01014f34> [ /lib/libpthread.so.0 + 0x4f34 ]

DCPLB_FAULT_ADDR: <0x0a7878bc> /* kernel dynamic memory */

ICPLB_FAULT_ADDR: <0x01014f34> [ /lib/libpthread.so.0 + 0x4f34 ]

 

PROCESSOR STATE:

R0 : 0a787878    R1 : 0a787878    R2 : 011177ff    R3 : 01117940

R4 : 01117a44    R5 : 011187ec    R6 : 00000830    R7 : fffffffe

P0 : 000000c4    P1 : 01018d94    P2 : 010480b0    P3 : 0a787878

P4 : 002d9b08    P5 : 002d9b08    FP : 0111788c    SP : 01115f24

LB0: 0115f891    LT0: 0115f890    LC0: 00000000

LB1: 0115d6b7    LT1: 0115d6b6    LC1: 00000000

B0 : 8000746e    L0 : 00000000    M0 : aae6b5ff    I0 : 0103ffe0

B1 : c0aa8890    L1 : 00000000    M1 : cb0039d3    I1 : 01049940

B2 : 0103ea14    L2 : 00000000    M2 : 8000746e    I2 : 0111af0c

B3 : 00000000    L3 : 00000000    M3 : 2402f7a1    I3 : 00000007

A0.w: 00000022   A0.x: 00000000   A1.w: 00000022   A1.x: 00000000

USP : 01117820  ASTAT: 02001004

 

Hardware Trace:

   0 Target : <0x0000508c> { _trap_c + 0x0 }

     Source : <0x00008bee> { _exception_to_level5 + 0xae } CALL pcrel

   1 Target : <0x00008b40> { _exception_to_level5 + 0x0 }

     Source : <0x000089fc> { _bfin_return_from_exception + 0x18 } RTX

   2 Target : <0x000089e4> { _bfin_return_from_exception + 0x0 }

     Source : <0x00008a98> { _ex_trap_c + 0x6c } JUMP.S

   3 Target : <0x00008910> { _ex_dcplb_miss + 0x0 }

     Source : <0x00008cba> { _trap + 0x5a } JUMP (P4)

   4 Target : <0x00008c60> { _trap + 0x0 }

     Source : <0x01014f30> [ /lib/libpthread.so.0 + 0x4f30 ] 0xe801

   5 Target : <0x01014f2e> [ /lib/libpthread.so.0 + 0x4f2e ]

     Source : <0x01018db8> [ /lib/libpthread.so.0 + 0x8db8 ] RTS

   6 Target : <0x01018db2> [ /lib/libpthread.so.0 + 0x8db2 ]

     Source : <0x01018dac> [ /lib/libpthread.so.0 + 0x8dac ] IF !CC JUMP

   7 Target : <0x01018da3> [ /lib/libpthread.so.0 + 0x8da3 ]

     Source : <0x01018db0> [ /lib/libpthread.so.0 + 0x8db0 ] JUMP.S

   8 Target : <0x01018dae> [ /lib/libpthread.so.0 + 0x8dae ]

     Source : <0x01018da7> [ /lib/libpthread.so.0 + 0x8da7 ]

   9 Target : <0x01018da2> [ /lib/libpthread.so.0 + 0x8da2 ]

     Source : <0x0000918c> { __common_int_entry + 0xcc } RTI

  10 Target : <0x0000912a> { __common_int_entry + 0x6a }

     Source : <0x00008e40> { _system_call + 0xb8 } RTS

  11 Target : <0x00008e3c> { _system_call + 0xb4 }

     Source : <0x00008e2c> { _system_call + 0xa4 } IF !CC JUMP

  12 Target : <0x00008e26> { _system_call + 0x9e }

     Source : <0x00008e16> { _system_call + 0x8e } IF !CC JUMP

  13 Target : <0x00008df6> { _system_call + 0x6e }

     Source : <0x00008fd4> { _schedule_and_signal_from_int + 0x34 } JUMP.S

  14 Target : <0x00008fd2> { _schedule_and_signal_from_int + 0x32 }

     Source : <0x000016ea> { _finish_atomic_sections + 0x32 } RTS

  15 Target : <0x000016e4> { _finish_atomic_sections + 0x2c }

     Source : <0x000016d4> { _finish_atomic_sections + 0x1c } IF !CC JUMP

Userspace Stack

Stack info:

SP: [0x01117820] <0x01117820> [ smb_test_bandwi + 0x820 ]

Memory from 0x01117820 to 01118000

01117820:[00000000] 00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117840: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117860: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117880: 00000000  00000000  00000000  01117a10 <016bbeb6> 017c1760  00000000  00000000

011178a0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

011178c0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

011178e0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117900: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117920: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117940: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117960: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117980: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

011179a0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

011179c0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

011179e0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117a00: 00000000  00000000  00000000  00000000  011190a4 <016bc23e> 002d9b08  002d5798

01117a20: 002d5798  00000830  011187ec  00000000  00000000  00000000  00000000  00000000

01117a40: 002f92e4  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117a60: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117a80: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117aa0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117ac0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117ae0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117b00: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117b20: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117b40: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117b60: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117b80: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117ba0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117bc0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117be0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117c00: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117c20: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117c40: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117c60: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117c80: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117ca0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117cc0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117ce0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117d00: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117d20: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117d40: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117d60: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117d80: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117da0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117dc0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117de0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117e00: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117e20: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117e40: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117e60: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117e80: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117ea0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117ec0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117ee0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117f00: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117f20: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117f40: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117f60: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117f80: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117fa0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117fc0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01117fe0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

Return addresses in stack:

    address : <0x016bbeb6> [ /home/smb_test_bandwidth + 0x2bbeb6 ]

    address : <0x016bc23e> [ /home/smb_test_bandwidth + 0x2bc23e ]

Bus error

 

 

 

With this message: DCPLB_FAULT_ADDR: <0x0a7878bc> /* kernel dynamic memory */

ICPLB_FAULT_ADDR: <0x01014f34> [ /lib/libpthread.so.0 + 0x4f34 ],The address in thread lib , How to fix the bug?

 

With bfin-linux-uclibc-g++ to compile code,it is not create *.gdb file,so how to get debug message ?

 

 

 

-Bil

QuoteReplyEditDelete

 

 

2010-05-26 00:11:12     Re: Some time write data to server failed using samaba

Mike Frysinger (UNITED STATES)

Message: 89851   

 

there is no need for a sep .gdb file with FDPIC because the file itself is the ELF

Attachments

Outcomes