2010-05-20 12:07:17     issues with linphone

Document created by Aaronwu Employee on Aug 21, 2013
Version 1Show Document
  • View in full screen mode

2010-05-20 12:07:17     issues with linphone

daniel amor (SPAIN)

Message: 89596   

 

Hi,

 

We are developing a product based in bfin and linphone. Our product is conected to an audio matrix with 3 different audio sources. Each audio source is associated to a VoIP extension, so when a call is stablished the remote party knows which audio source is generating the call.

 

 

 

Now I'm using release 2009R1.1-RC4 and BF536 Rev 0.2. I'm facing some problems with linphone. I'll explain the steps taken, the problems found and the solution used.

 

 

 

I used the linphone 3.0.0 provided with the distribution, this linphone had the problem that when registering more than one proxy sometimes I got this message "Unauthorized To header", looking at the traffic with wireshark we found that in the register information sent to the server there was a mismatch between the username and the sip uri, It was something like this:

 

sip:dd3@sip.antisip.com

 

username: dd1

 

 

 

I took linphone 3.1.2 from trunk and got the same problem. The following I did was taking official linphone, versions 3.2.0 and 3.3.0. In the first one I had to apply the vfork patch, the second had it included.

 

 

 

Those two versions didn't show the authentication problem, but those versions had another big problem. When calling to a remote party it didn't mind which proxy identity was being used, It always used the first one registered.

 

 

 

Finally, I took the file coreapi/authentication.c from version 3.2.0 and placed it in version 3.1.2 and version 3.0.0 . Now those early versions register the extensions correctly and the remote names are OK.

 

 

 

Could anybody confirm this behaviour?

 

 

 

Thanks for all,

 

 

 

  Daniel,

TranslateQuoteReplyEditDelete

 

 

2010-05-20 13:21:18     Re: issues with linphone

Robin Getz (UNITED STATES)

Message: 89597   

 

Daniel:

 

You might be better off on the linphone mailing list - did you try there?

 

-Robin

QuoteReplyEditDelete

 

 

2010-05-20 13:32:15     Re: issues with linphone

daniel amor (SPAIN)

Message: 89598   

 

Hi,

 

  I am in the process of placing this issue there too, I only wanted to coment it here in case anybody is in the same situation as me.

 

Thanks,

Attachments

    Outcomes