2010-04-29 02:43:25     uClinux-Console using netcat (nc)

Document created by Aaronwu Employee on Aug 21, 2013
Version 1Show Document
  • View in full screen mode

2010-04-29 02:43:25     uClinux-Console using netcat (nc)

Patrick Hotz (GERMANY)

Message: 89004   

 

Hi,

 

a few days ago i have found a very good function in the u-boot which uses the netcat (nc) protocoll to send the stdin and stdout to my pc.

 

 

My question is following: Is there a function in uClinux which is using the same way (nc) to send the "console" to my pc?

 

Thanks,

Patrick

TranslateQuoteReplyEditDelete

 

 

2010-04-29 03:05:42     Re: uClinux-Console using netcat (nc)

Mike Frysinger (UNITED STATES)

Message: 89006   

 

please search/read the documentation:

  docs.blackfin.uclinux.org/doku.php?id=linux-kernel:netconsole

QuoteReplyEditDelete

 

 

2010-05-11 06:28:21     Re: uClinux-Console using netcat (nc)

Patrick Hotz (GERMANY)

Message: 89320   

 

Hi,

 

i have currently running the netconsole as build in and this seems to be working.

This is my bootarg: "netconsole=6665@192.168.10.226/eth0,6666@192.168.10.224/" (226 is my device / 224 is my PC)

 

If i boot the device i can see the boot-printouts but the outputs from the rc-script and the "normal" console is nothing...

Also if i want to write someting to my remote-console there is nothing happening...

 

I use "netcat -u -l -p 6666" on my PC.

 

 

 

Is there any trick i can try?

TranslateQuoteReplyEditDelete

 

 

2010-05-11 13:32:57     Re: uClinux-Console using netcat (nc)

Mike Frysinger (UNITED STATES)

Message: 89321   

 

please read the documentation i already pointed you to.  the very first intro paragraph cleary explains this behavior.

Attachments

    Outcomes