2010-05-10 10:07:10     在bf533-Ezkit上使用microwindows出错

Document created by Aaronwu Employee on Aug 21, 2013
Version 1Show Document
  • View in full screen mode

2010-05-10 10:07:10     在bf533-Ezkit上使用microwindows出错

进 王 (CHINA)

Message: 89283   

 

大家好,我用的开发板是BF533-Ezkit,编译的内核文件是uClinux-dist-2008R1-RC8,配置好一切后现在板子上运行microwindows,出现如下问题,

root:/> nano-X &

175

root:/> m. Check kernel config

Cannot initialise screen

请问我该如何解决,谢谢!

TranslateQuoteReplyEditDelete

 

 

2010-05-10 11:19:27     在bf533-Ezkit上使用microwindows出错

Mike Frysinger (UNITED STATES)

Message: 89285    you need to actually describe your hardware setup. the bf533-ezkit

has no LCD by default, so nano-X isnt going to make sense/work there.

 

also, 2008R1 is old. use the latest release.

QuoteReplyEditDelete

 

 

2010-05-11 01:42:41     Re: 在bf533-Ezkit上使用microwindows出错

进 王 (CHINA)

Message: 89300   

 

我的硬件是System Stater Kit_BF533 DSP教学开发系统,它是由ADSP-BF533 EZKIT评估板和DM-KIT-SSK扩展卡组成的,有一个320*240的带触屏的24位色TFT液晶屏。

 

我会试一下最新的系统,谢谢!

TranslateQuoteReplyEditDelete

 

 

2010-05-11 02:33:53     Re: 在bf533-Ezkit上使用microwindows出错

Mike Frysinger (UNITED STATES)

Message: 89301   

 

i'm pretty sure no one has ever tested that display.  there probably isnt even an LCD driver which means things like nano-X have no chance of working.

 

you'll need to write a driver first.  i.e. use video_test to verify functionality before doing anything else.

Attachments

    Outcomes