2010-04-20 10:31:45     Confused about uImage for BF537 STAMP

Document created by Aaronwu Employee on Aug 21, 2013
Version 1Show Document
  • View in full screen mode

2010-04-20 10:31:45     Confused about uImage for BF537 STAMP

Bo Li (CHINA)

Message: 88650   

 

    uImage-bf537-stamp-2009R1.1-RC4 is size of 4.5MB, while the size of flash memory on BF537 EZ-Kit is only 4MB. So the problem is: how can I write this image into flash in order to boot the OS automaticly when the board power is on? Just now I can only download it from the host by tftp.

 

    And may someone give a link about how to and where to write the uclinux image into the flash on board? Thank you in advance.

 

    Regards,

 

Libo

QuoteReplyEditDelete

 

 

2010-04-20 10:38:54     Re: Confused about uImage for BF537 STAMP

Bo Li (CHINA)

Message: 88652   

 

Ok, I check out there is nand flash on this board. I'll try work on this.

QuoteReplyEditDelete

 

 

2010-04-20 11:03:18     Re: Confused about uImage for BF537 STAMP

Bo Li (CHINA)

Message: 88655   

 

Ok, I check out there is nand flash on this board. I'll try work on this.

 

---Got really confused, there no detailed explaination on Nand --U39-43. Need your help.

 

QuoteReplyEditDelete

 

 

2010-04-20 13:43:30     Re: Confused about uImage for BF537 STAMP

Robin Getz (UNITED STATES)

Message: 88659   

 

Libo:

 

The default images were never ment to be burned to flash. They are ment to be transfered to the board over the network, and booted. If you want a custom image that can be burned into flash - that is up to you to build.

 

-Robin

QuoteReplyEditDelete

 

 

2010-04-20 15:38:21     Re: Confused about uImage for BF537 STAMP

Mike Frysinger (UNITED STATES)

Message: 88661   

 

i dont know where you keep looking, but none of the things you mention are on the board.  the bf537-stamp/ezkit have no nand flash.

Attachments

    Outcomes