2010-04-15 04:17:09     compiling uCLinux for SRV1 problem

Document created by Aaronwu Employee on Aug 21, 2013
Version 1Show Document
  • View in full screen mode

2010-04-15 04:17:09     compiling uCLinux for SRV1 problem

Dan Novischi (ROMANIA)

Message: 88443   

 

Hi,

 

I'm trying to compile the uCLinux distrib. for my SRV1 robot, but i haven't haven't had any success yet.

 

I have the the following toolchain installed:

 

bfin-uclinux-gcc -v

 

 

Using built-in specs.

Target: bfin-uclinux

Configured with: /usr/src/packages/BUILD/blackfin-toolchain-09r1.1/../gcc-4.1/configure --build=i686-pc-linux-gnu --host=i686-pc-linux-gnu --target=bfin-uclinux --prefix=/opt/uClinux/bfin-uclinux --enable-threads=posix --with-sysroot=/opt/uClinux/bfin-uclinux/bfin-uclinux/runtime --disable-libstdcxx-pch --disable-symvers --disable-libssp --disable-libffi --enable-clocale=generic --enable-version-specific-runtime-libs --enable-__cxa_atexit --with-bugurl=URL:  blackfin.uclinux.org/gf/project/toolchain/tracker --with-pkgversion=ADI-09r1.1-2

Thread model: posix

gcc version 4.1.2 (ADI svn)

 

 

Within the "make meniuconfig" i have chosen Vendors->Surveyor->SRV1 and the Minotaur board (after reading this:   www.surveyor.com/cgi-bin/yabb2/YaBB.pl?num=1268233315/5#5 ).

 

After that i tried "make clean" than "make 2>log.err".

 

log.err

QuoteReplyEditDelete

 

 

2010-04-15 04:20:44     Re: compiling uCLinux for SRV1 problem

Dan Novischi (ROMANIA)

Message: 88444   

 

Can anyone help me to resolve this problem?

 

Thank you so much,

 

Dan.

QuoteReplyEditDelete

 

 

2010-04-15 12:03:05     Re: compiling uCLinux for SRV1 problem

Mike Frysinger (UNITED STATES)

Message: 88460   

 

do not pester for answers a mere three minutes after posting the original question

QuoteReplyEditDelete

 

 

2010-04-15 12:06:15     Re: compiling uCLinux for SRV1 problem

Mike Frysinger (UNITED STATES)

Message: 88461   

 

looks like the surveyor guys never created a dedicated board file for the kernel.  one needs to be created for it.

QuoteReplyEditDelete

 

 

2010-04-15 12:26:37     Re: compiling uCLinux for SRV1 problem

Mike Frysinger (UNITED STATES)

Message: 88464   

 

i dont know why your system picked the minotaur board by default, but you can try changing the selection yourself in the kernel config to the sTAMP board

QuoteReplyEditDelete

 

 

2010-04-15 15:53:40     Re: compiling uCLinux for SRV1 problem

Dan Novischi (ROMANIA)

Message: 88479   

 

Thanks so much for the info, for the stamp board i can compile fine! I hope it works with my SRV1.

 

Thank you a million!

Attachments

Outcomes