2010-02-15 07:40:32     Kernel panic - mounted Fat32 HDD browse

Document created by Aaronwu Employee on Aug 20, 2013Last modified by Aaronwu Employee on Aug 20, 2013
Version 2Show Document
  • View in full screen mode

2010-02-15 07:40:32     Kernel panic - mounted Fat32 HDD browse

Jayakumar Ananthakrishnan (INDIA)

Message: 86106   

 

Hi,

 

I have mounted a HDD (Fat32 format) after the kernel boot-up.

 

When I press tab key after typing the following command "rm -rf mnt/usb/NP" in the root level, I am getting a kernel panic.

 

Could anybody tell me what could be the reason for this. I am using 2009RC1 package.

 

P.S KernelPanic_Browse.tar.gz log attached

 

Thanks in advance,

 

Regards,

 

Jai

 

KernelPanic_Browse.tar.gz

QuoteReplyEditDelete

 

 

2010-02-15 11:07:31     Re: Kernel panic - mounted Fat32 HDD browse

Robin Getz (UNITED STATES)

Message: 86119   

 

Jai:

 

Did you see the "utf8 is not a recommended IO charset for FAT filesystems"?

 

Do you get this all the time? or just random times?

 

-Robin

QuoteReplyEditDelete

 

 

2010-02-15 13:35:47     Re: Kernel panic - mounted Fat32 HDD browse

Jayakumar Ananthakrishnan (INDIA)

Message: 86123   

 

Robin,

 

Yes I always see utf8 warning message whenever I mount a drive in fat format with iocharset = utf8.

 

I get kernel panic randomly.

 

~Jai

QuoteReplyEditDelete

 

 

2010-02-15 13:50:32     Re: Kernel panic - mounted Fat32 HDD browse

Robin Getz (UNITED STATES)

Message: 86125   

 

Jai:

 

Do you see the same thing on other platforms? or just yours? It could be a hardware (memory) issue.

 

-Robin

QuoteReplyEditDelete

 

 

2010-02-16 00:43:42     Re: Kernel panic - mounted Fat32 HDD browse

Jayakumar Ananthakrishnan (INDIA)

Message: 86132   

 

Robin,

 

If this thread can be tracked with Fat panic issue thread posted by me, then please close this thread.

 

Please let me know if there are any test suite to test my low-level drivers to confirm if it is a hardware issue.

 

~jai

Attachments

Outcomes