2010-01-29 01:22:23     Driver Support 0n 2008R1.5

Document created by Aaronwu Employee on Aug 20, 2013
Version 1Show Document
  • View in full screen mode

2010-01-29 01:22:23     Driver Support 0n 2008R1.5

vijai ragavan (INDIA)

Message: 85274   

 

Dear All,

 

I need to know whether 2008 R1.5 supports the following driver or not.

 

Flash driver(S29GL512P(128MB)-16Bit)

 

Ethernet driver(LAN9218)

 

USB driver(R8A66597FP)

 

SDRAM(MT48LC32M16A2TG-7E(128MB))

 

Please suggest.

 

 

 

Thanks&Regards,

 

Vijayaragavan.S

QuoteReplyEditDelete

 

 

2010-01-29 01:44:34     Re: Driver Support 0n 2008R1.5

Mike Frysinger (UNITED STATES)

Message: 85277   

 

we dont maintain exhaustive lists of drivers and what existed in which release.  we'd have to read the source code just like you to figure out whether a driver existed.

 

off the top of my head, SDRAM type is irrelevant to Linux and pretty much to u-boot.  it's up to you to program the timings yourself.

 

the latest release should support all the LAN9{1,2}1x SMSC ethernet parts in the smc911x driver.

 

read the spec on the flash part.  if it's CFI, it probably works.

 

look in the usb directory to see if that USB part is supported.

QuoteReplyEditDelete

 

 

2010-01-29 05:50:25     Re: Driver Support 0n 2008R1.5

vijai ragavan (INDIA)

Message: 85321   

 

Thanks for the support

Attachments

    Outcomes