2010-01-07 19:05:01     BUG: failure at mm/nommu.c:127/kobjsize()!

Document created by Aaronwu Employee on Aug 20, 2013
Version 1Show Document
  • View in full screen mode

2010-01-07 19:05:01     BUG: failure at mm/nommu.c:127/kobjsize()!

Terry Bartholomew (UNITED STATES)

Message: 84285   

 

Hello,

 

The scenario:  issuing a ps command for process list returns a partial process list, then the following error:

 

BUG: failure at mm/nommu.c:127/kobjsize()!

Kernel panic - not syncing: BUG!

 

CPU:   ADSP bf537-0.2 (Detected Rev: 0.3)

Linux version 2.6.22.19-ADI-2008R1.5-svn622

 

Suggestions?

 

thanks,

 

Terry

QuoteReplyEditDelete

 

 

2010-01-07 20:35:40     Re: BUG: failure at mm/nommu.c:127/kobjsize()!

Yi Li (CHINA)

Message: 84287   

 

Terry,

 

Could you try latest release 2009R1.1-RC4? Also compile kernel for bf527 rev 0.3.

 

-Yi

QuoteReplyEditDelete

 

 

2010-01-07 20:59:19     Re: BUG: failure at mm/nommu.c:127/kobjsize()!

Terry Bartholomew (UNITED STATES)

Message: 84288   

 

Hi Yi,

 

Thank you!    I will make your suggestion to the vendor.  Is the ps BUG failure a known error  for the version I listed?

 

-Terry

QuoteReplyEditDelete

 

 

2010-01-07 21:16:47     Re: BUG: failure at mm/nommu.c:127/kobjsize()!

Yi Li (CHINA)

Message: 84289   

 

Terry,

 

This is an old bug (see: https://blackfin.uclinux.org/gf/tracker/1233) but it is already fixed in later 2008R1.5 release. But I would suggest to use 2009R1.1-RC4, since 2008R1.5 is not supported any more.

 

-Yi

Attachments

    Outcomes