2009-12-17 17:05:49     Can I force driver to use SPORT instead SPI? (enc28j60)

Document created by Aaronwu Employee on Aug 20, 2013
Version 1Show Document
  • View in full screen mode

2009-12-17 17:05:49     Can I force driver to use SPORT instead SPI? (enc28j60)

Rafal Osinski (POLAND)

Message: 83649   

 

Hello,

 

I`ve got ethernet enc28j60 driver builded as module, when i modprobe it - it uses 'standard' SPI, how can i force it to use SPORT1 emulatet as SPI? I use BF561 EzKit

 

thanks for your help

 

Rafal Osinski

QuoteReplyEditDelete

 

 

2009-12-17 17:16:18     Re: Can I force driver to use SPORT instead SPI? (enc28j60)

Mike Frysinger (UNITED STATES)

Message: 83650   

 

the bus a device is connected to is controlled in the platform resources

QuoteReplyEditDelete

 

 

2009-12-21 12:01:47     Re: Can I force driver to use SPORT instead SPI? (enc28j60)

Rafal Osinski (POLAND)

Message: 83797   

 

does anyone know is there a platform resources definied for a board in witch SPORT is definied as SPI bus (i need some example to look at and understand it), and resources neaded for ENC28j60?

 

thanks for help

QuoteReplyEditDelete

 

 

2009-12-21 12:06:44     Re: Can I force driver to use SPORT instead SPI? (enc28j60)

Mike Frysinger (UNITED STATES)

Message: 83798   

 

grep bfin-sport-spi arch/blackfin/mach-*/boards/*.c

Attachments

    Outcomes