2009-11-16 05:45:29     Sending/Receiving Can Messages

Document created by Aaronwu Employee on Aug 19, 2013
Version 1Show Document
  • View in full screen mode

2009-11-16 05:45:29     Sending/Receiving Can Messages

Andy Cullen (IRELAND)

Message: 82413   

 

Hi all,

 

I need to send and receive CAN messages using the Blackfin BF 537 Stamp Board via the command line (i.e. I have FTPed in). Does anyone have a simple run down of how to do this or can direct me in the right direction?

 

The blackfin baord is mounted onto a robot which has seperate modules controlling each element of the robot. The modules have CAN Bus functionality and work fine. The only interface I have is the command line of the blackfin board and once a succesful message is send then i should be able to get it to move or speak or wink etc. I am just having trouble getting the command from my laptop to the board.

 

Any help is very much appriciated

 

Thanks,

 

Andy

QuoteReplyEditDelete

 

 

2009-11-16 11:07:28     Re: Sending/Receiving Can Messages

Robin Getz (UNITED STATES)

Message: 82416   

 

Andy:

 

Linux questions should be asked in the Linux forums - not the hardware ones.

 

-Robin

QuoteReplyEditDelete

 

 

2009-11-16 11:20:37     Re: Sending/Receiving Can Messages

Mike Frysinger (UNITED STATES)

Message: 82417   

 

ive just been moving threads lately for people ...

QuoteReplyEditDelete

 

 

2009-11-16 21:00:55     Re: Sending/Receiving Can Messages

Barry Song (CHINA)

Message: 82422   

 

Andy,

 

Pls refer to

 

  docs.blackfin.uclinux.org/doku.php?id=linux-kernel:drivers:can_module

 

-barry

Attachments

    Outcomes