2009-11-13 01:26:33     make error: {standard input}: Assembler messages

Document created by Aaronwu Employee on Aug 19, 2013
Version 1Show Document
  • View in full screen mode

2009-11-13 01:26:33     make error: {standard input}: Assembler messages

baihuawen xiao (CHINA)

Message: 82339   

 

when I try to port gnokii to blackfin, I got the following messages during compiling.

 

/tmp/ccjj8jZU.s: Assembler messages:

/tmp/ccjj8jZU.s:222: Error: syntax error. Input text was cld.

/tmp/ccjj8jZU.s:222: Error:

/tmp/ccjj8jZU.s:222: Error: syntax error. Input text was rep.

/tmp/ccjj8jZU.s:222: Error:

/tmp/ccjj8jZU.s:222: Error: syntax error. Input text was stosl.

/tmp/ccjj8jZU.s:222: Error:

/tmp/ccjj8jZU.s:227: Error: syntax error. Input text was btsl.

/tmp/ccjj8jZU.s:227: Error:

/tmp/ccjj8jZU.s:298: Error: syntax error. Input text was cld.

/tmp/ccjj8jZU.s:298: Error:

/tmp/ccjj8jZU.s:298: Error: syntax error. Input text was rep.

/tmp/ccjj8jZU.s:298: Error:

/tmp/ccjj8jZU.s:298: Error: syntax error. Input text was stosl.

/tmp/ccjj8jZU.s:298: Error:

/tmp/ccjj8jZU.s:307: Error: syntax error. Input text was btsl.

/tmp/ccjj8jZU.s:307: Error:

 

Could anybody help to fix it,

 

Thanks.

TranslateQuoteReplyEditDelete

 

 

2009-11-13 04:19:17     Re: make error: {standard input}: Assembler messages

Yi Li (CHINA)

Message: 82353   

 

Baihuawen,

 

Please tell us the detail steps to reproduce your problem.

 

-Yi

QuoteReplyEditDelete

 

 

2009-11-13 10:03:22     Re: make error: {standard input}: Assembler messages

Mike Frysinger (UNITED STATES)

Message: 82358   

 

either you misconfigured gnokii, or it assumes an x86 target.  it's trying to compile x86 asm instructions which obviously wont work for a blackfin target.

QuoteReplyEditDelete

 

 

2009-11-16 04:54:27     Re: make error: {standard input}: Assembler messages

baihuawen xiao (CHINA)

Message: 82411   

 

Thanks for your help.

 

But when I configure it,I use "--host=bfin-uclinux ", it says:

 

checking build system type... i686-pc-linux-gnu

checking host system type... bfin-unknown-uclinux

checking target system type... bfin-unknown-uclinux

checking for bfin-uclinux-gcc... bfin-linux-uclibc-gcc

checking for C compiler default output file name... a.out

checking whether the C compiler works... yes

checking whether we are cross compiling... yes

 

And when compiling, it use bfin-linux-uclibc-gcc as:

 

bfin-linux-uclibc-gcc -DHAVE_CONFIG_H -I. -I../include   -DEMBED -D__uClinux__ -I/home/ji

anxiao/others/svn/uclinux-dist-trunk-svn-7715  -mcpu=bf527-0.0 -I/usr/include  -O3 -Wall

-Wno-pointer-sign -fvisibility=hidden -fno-strict-aliasing  -c getopt1.c

 

Is there anything error?

 

Thanks again.

TranslateQuoteReplyEditDelete

 

 

2009-11-16 19:33:06     Re: make error: {standard input}: Assembler messages

Mike Frysinger (UNITED STATES)

Message: 82421   

 

the package is inserting -I/usr/include which will cause build errors.  you'll have to find & fix that.  try grepping the Makefile.

Attachments

    Outcomes