2009-10-18 12:00:13     BF537 connection to SATA-HDD

Document created by Aaronwu Employee on Aug 19, 2013
Version 1Show Document
  • View in full screen mode

2009-10-18 12:00:13     BF537 connection to SATA-HDD

Patrick Hotz (GERMANY)

Message: 81411   

 

Hi,

 

i have only a small question,

I have seen that it is possible to connect a SATA-HDD (maybe also a IDE-HDD) to the Blackfin but i havn´t found any schematic for this.

 

Where can i find this and is there a running driver in uClinux?

 

 

 

greetings,

Patrick

TranslateQuoteReplyEditDelete

 

 

2009-10-18 13:56:46     Re: BF537 connection to SATA-HDD

Mike Frysinger (UNITED STATES)

Message: 81412   

 

we've never done anything with SATA (hardware or software).  one or two people in the forums talked about working on it, but that's about it.

QuoteReplyEditDelete

 

 

2009-10-18 14:30:16     Re: BF537 connection to SATA-HDD

Patrick Hotz (GERMANY)

Message: 81413   

 

OK, thank you.

 

I will try it with a USB-SATA adapter on my board.

 

Patrick

TranslateQuoteReplyEditDelete

 

 

2009-10-18 14:36:51     Re: BF537 connection to SATA-HDD

Patrick Hotz (GERMANY)

Message: 81414   

 

by the way,

 

do you have ever tried the AT43301 USB-Hub Chip (5-Port) on the SL811HST ?

 

Patrick

TranslateQuoteReplyEditDelete

 

 

2009-10-18 23:25:47     Re: BF537 connection to SATA-HDD

Sonic Zhang (CHINA)

Message: 81419   

 

SATA DH should work with the IDE/CF/NAND add-on board on bf537 via a IDE2SATA convert board, if you use 2009R1 release.

QuoteReplyEditDelete

 

 

2009-10-19 02:29:27     Re: BF537 connection to SATA-HDD

Patrick Hotz (GERMANY)

Message: 81426   

 

Hi,

 

i will try it with both versions.

First the USB-SATA and in the next step IDE-SATA.....

 

For schematic i can use the 0.8 rel (CF_-_IDE_ATA_-_NAND-Schematic_Prints_v08_REL.pdf) ?

Is is save to use it?

 

 

 

Patrick

TranslateQuoteReplyEditDelete

Attachments

    Outcomes