2009-09-26 15:43:11     Latest uCLinux: no support for ADI boards other than Coyote?

Document created by Aaronwu Employee on Aug 19, 2013
Version 1Show Document
  • View in full screen mode

2009-09-26 15:43:11     Latest uCLinux: no support for ADI boards other than Coyote?

Amusing Muses (CANADA)

Message: 80495   

 

Hi I have a BF533 EZKIT that I'm trying to get Linux on to (despite the wiki saying that Blackfin Linux developers typically do not use this platform[1] and claiming that the flash is too small for a default uImage...).

 

So I downloaded the latest uCLinux (uClinux-dist-20090618.tar.bz2) and started to configure it but when I do

 

make menuconfig

 

And l choose Vendor->ADI then the only option under ADI Products is "Coyote".

 

Shouldn't there be a lot more options under here? Or are all the boards that are supposed to be supported on this site actually a part of some kind of fork off of the main uCLinux distribution? If so, where can I find the source for the latest uCLinux that I can customize for my BF533-EZKIT LITE?

 

Thanks.

 

Reference:

 

[1]:   docs.blackfin.uclinux.org/doku.php?id=hw:boards:bf533-ezkit

QuoteReplyEditDelete

 

 

2009-09-26 16:39:30     Re: Latest uCLinux: no support for ADI boards other than Coyote?

Mike Frysinger (UNITED STATES)

Message: 80496   

 

download the dist from our website, not the common uclinux one.  the ADI vendor is not "ADI", it's "Analog Devices".

QuoteReplyEditDelete

 

 

2009-09-26 20:23:14     Re: Latest uCLinux: no support for ADI boards other than Coyote?

Amusing Muses (CANADA)

Message: 80500   

 

Sure no problem, done, now just one question: Why do the sources occupy 6.2G?

 

 

du -sh uclinux-dist/

6.2G    uclinux-dist/

 

 

No wonder it took so long to fetch... Why's it so big?

 

Thanks.

QuoteReplyEditDelete

 

 

2009-09-26 23:09:47     Re: Latest uCLinux: no support for ADI boards other than Coyote?

Mike Frysinger (UNITED STATES)

Message: 80507   

 

because there's a lot of packages

QuoteReplyEditDelete

Attachments

    Outcomes