2009-09-24 03:52:29     Problem with recored file while transfering to the windows after arecord

Document created by Aaronwu Employee on Aug 19, 2013
Version 1Show Document
  • View in full screen mode

2009-09-24 03:52:29     Problem with recored file while transfering to the windows after arecord

Vikram Chowdhari (INDIA)

Message: 80365   

 

Hi !

 

I have recored a file for around 10 sec .wav file. using codec 1854 and 1871 in BF537. While rcp to the system the duration of the fie increases ( more than 10sec) the clarity of the audio clip also goes bad. I am using this method for the linphone application. Could anyone tell me as what is the problem.

 

 

 

Thnaks in advance

 

Vikram

QuoteReplyEditDelete

 

 

2009-09-24 10:22:55     Re: Problem with recored file while transfering to the windows after arecord

Robin Getz (UNITED STATES)

Message: 80384   

 

Vikram:

 

I'm not sure what you are saying.

 

The act of transfering the file from the blackfin to the host via rcp causes the file size to increase?

 

-Robin

Attachments

    Outcomes