2009-09-23 03:12:57     debugging kernel using kgdb over JTAG

Document created by Aaronwu Employee on Aug 19, 2013
Version 1Show Document
  • View in full screen mode

2009-09-23 03:12:57     debugging kernel using kgdb over JTAG

Manu AS (INDIA)

Message: 80273   

 

Hi

 

I want to enable kernel debugging using gdb over JTAG.

 

Following are some of the config details:

 

Target HW: bf561 based dev board

 

uClinux distribution: 2008R1

 

JTAG device: ADDS-HPUSB-ICE

 

Can some body tell me the steps for the same.

 

Thanks

QuoteReplyEditDelete

 

 

2009-09-23 10:05:55     Re: debugging kernel using kgdb over JTAG

Mike Frysinger (UNITED STATES)

Message: 80309   

 

as the documentation states, the HPUSB ICE is not supported.  further, kgdb is a software-only debugger which means it makes no sense to use it with jtag.

 

if you want to debug the kernel via jtag, go buy a gnICE.

QuoteReplyEditDelete

 

 

2009-09-24 00:16:08     Re: debugging kernel using kgdb over JTAG

Manu AS (INDIA)

Message: 80327   

 

Thanks Mike.

Attachments

    Outcomes