2009-09-18 09:09:45     problems microwindows nano-X

Document created by Aaronwu Employee on Aug 19, 2013
Version 1Show Document
  • View in full screen mode

2009-09-18 09:09:45     problems microwindows nano-X

Patrick Hotz (GERMANY)

Message: 80137   

 

Hi,

 

maybe i have written this a few months ago but i think this is important for everyone who wants to use nano-X...

 

 

 

The config in uCLinux "microwindows" - "Screen PixType" is without any change in the nano-X application.....

For example:

     I set it to "Packet-16bit-5/6/5", "make clean;make" and run "nano-X" on my blackfin.....

     but the "nano-X" wants to set a color-palette of 16 Colors...and that is not 16Bit !!!!!!!!!!!!

 

 

 

Also there is a problem with fltk...

    If i draw a Fl-Image the image is distored in a angle of 45° ( a | line is \ )....

 

 

 

Regards,

Patrick

Attachments

    Outcomes