2009-08-18 03:16:37     接刚才无法启动JFFS2文件启动

Document created by Aaronwu Employee on Aug 16, 2013
Version 1Show Document
  • View in full screen mode

2009-08-18 03:16:37     接刚才无法启动JFFS2文件启动

杨 永标 (CHINA)

Message: 78975   

 

我操作过程如下

 

1 按说明配置menuconfig 然后make ,将image下的rootfs.jffs2(约2M大小文件系统),和vmImage(约0.96M)拷贝到出来.

 

2 将vmImage写入0x20000000开始地址

 

3将rootfs.jffs2写入0x20100000开始地址

 

4

 

setenv bootargs root=/dev/mtdblock2 rw rootfstype=jffs2

 

setenv flashboot bootm 0x20000000

 

setenv bootcmd run flashboot

 

 

5 上电无法启动

 

Booting kernel from Legacy Image at 20000000 ...

   Image Name:   Linux-2.6.28.10-ADI-2009R1

   Created:      2009-08-18   6:47:42 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    1004041 Bytes = 980.5 kB

   Load Address: 00001000

   Entry Point:  001beba4

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 001beba4

 

一直在等待,一直无法进行下去

TranslateQuoteReplyEditDelete

 

 

2009-08-18 03:30:09     Re: 接刚才无法启动JFFS2文件启动

Yi Li (CHINA)

Message: 78978   

 

同一问题请不要反复提问。如果kernel hang住,请debug:   docs.blackfin.uclinux.org/doku.php?id=linux-kernel:debug:post_mortem

QuoteReplyEditDelete

 

 

2009-08-18 03:36:35     Re: 接刚才无法启动JFFS2文件启动

杨 永标 (CHINA)

Message: 78979   

 

不好意思,网速慢,一下子出现了发了三个

TranslateQuoteReplyEditDelete

Attachments

    Outcomes