2009-08-10 20:51:22     svn: Can't connect to host 'firewall-sources.blackfin.uclinux.org': Connection refused

Document created by Aaronwu Employee on Aug 16, 2013
Version 1Show Document
  • View in full screen mode

2009-08-10 20:51:22     svn: Can't connect to host 'firewall-sources.blackfin.uclinux.org': Connection refused

Frank Van Hooft (CANADA)

Message: 78578   

 

I'm installing the tools and code on a new machine (Ubuntu 9.04) and am having some troubles getting the svn uclinux code.

 

Running this with an empty uclinux-dist directory:

 

svn checkout svn://sources.blackfin.uclinux.org/uclinux-dist/branches/2009R1 uclinux-dist

 

results in a checkout that runs for about an hour or so, downloading a boatload of code, then abruptly terminating with the message:

 

svn: Can't connect to host 'firewall-sources.blackfin.uclinux.org': Connection refused

 

Repeated attempts, or doing an "svn up" just yield the same result. I thought perhaps it was an ubuntu 9 thing, so I also tried an "svn up" on my svn trunk directory on the ubuntu 7 machine and saw the same message. Which is funny because the ubuntu 7 machine had been the main development machine for a long time; it had never had a problem.

 

Taking a look at my uclinux-dist directory, this is what I see:

 

 

total 116

drwxr-xr-x   8 frank frank  4096 2009-08-10 15:38 bfin_patch

drwxr-xr-x   3 frank frank  4096 2009-08-10 16:23 bin

drwxr-xr-x   4 frank frank  4096 2009-08-10 15:38 config

-rw-r--r--   1 frank frank 18007 2009-08-10 17:13 COPYING

drwxr-xr-x   4 frank frank  4096 2009-08-10 16:23 Documentation

drwxr-xr-x  12 frank frank  4096 2009-08-10 16:24 freeswan

drwxr-xr-x 105 frank frank  4096 2009-08-10 16:23 lib

-rwxr-xr-x   1 frank frank  1967 2009-08-10 17:13 MAKEALL

-rw-r--r--   1 frank frank 15877 2009-08-10 17:13 Makefile

drwxr-xr-x  15 frank frank  4096 2009-08-10 15:38 openswan

-rw-r--r--   1 frank frank  5886 2009-08-10 17:13 README

-rw-r--r--   1 frank frank 10331 2009-08-10 17:13 release_notes

-rw-r--r--   1 frank frank  1743 2009-08-10 17:13 SOURCE

drwxr-xr-x 117 frank frank  4096 2009-08-10 16:26 testsuites

drwxr-xr-x   7 frank frank  4096 2009-08-10 15:38 tools

drwxr-xr-x 299 frank frank 12288 2009-08-10 17:13 user

drwxr-xr-x  74 frank frank  4096 2009-08-10 15:33 vendors

 

 

 

 

 

Note the absence of a linux-2.6.x directory.

 

I've had no problems obtaining the tools, or u-boot. It's only been the uclinux code.

 

Any suggestions would be appreciated.

 

Thanks.

QuoteReplyEditDelete

 

 

2009-08-10 21:04:41     Re: svn: Can't connect to host 'firewall-sources.blackfin.uclinux.org': Connection refused

Mike Frysinger (UNITED STATES)

Message: 78579   

 

should be fixed now.  port conflict prevented proper startup of svnserve on that port.

QuoteReplyEditDelete

 

 

2009-08-10 23:08:43     Re: svn: Can\\\'t connect to host \\\'firewall-sources.blackfin.uclinux.org\\\': Connection refused

Frank Van Hooft (CANADA)

Message: 78584   

 

Looks like you fixed it - "svn up" is running now & creating a linux-2.6.x directory. Thanks Mike.

Attachments

    Outcomes