2009-08-10 09:17:42     isp1362_hc_reset: Clock not ready after 100ms

Document created by Aaronwu Employee on Aug 16, 2013
Version 1Show Document
  • View in full screen mode

2009-08-10 09:17:42     isp1362_hc_reset: Clock not ready after 100ms

Chunbo Fan (CHINA)

Message: 78559   

 

hi everyone!

 

      my target board is ezkit-bf533 and the usb host controller is isp 1362

 

    // ezkit.c

 

#if defined(CONFIG_USB_ISP1362_HCD) || defined(CONFIG_USB_ISP1362_HCD_MODULE)

static struct resource isp1362_hcd_resources[] = {

    {

        .start = 0x20330000,

        .end = 0x20330000,

        .flags = IORESOURCE_MEM,

    }, {

        .start = 0x20330004,

        .end = 0x20330004,

        .flags = IORESOURCE_MEM,

    }, {

        .start = IRQ_PF5,

        .end = IRQ_PF5,

        .flags = IORESOURCE_IRQ | IORESOURCE_IRQ_HIGHLEVEL,

 

    },

};

 

static struct isp1362_platform_data isp1362_priv = {

    .sel15Kres = 1,

    .clknotstop = 0,

    .oc_enable = 0,

    .int_act_high =0,

    .int_edge_triggered =0,

    .remote_wakeup_connected = 0,

    .no_power_switching = 1,

    .power_switching_mode = 0,

};

 

static struct platform_device isp1362_hcd_device = {

    .name = "isp1362-hcd",

    .id = 0,

    .dev = {

        .platform_data = &isp1362_priv,

    },

    .num_resources = ARRAY_SIZE(isp1362_hcd_resources),

    .resource = isp1362_hcd_resources,

};

#endif

 

 

 

when I reboot the system,I found the error like this:

 

driver isp1362-hcd, 2005-04-04

isp1362-hcd isp1362-hcd.0: ISP1362 Host Controller

isp1362-hcd isp1362-hcd.0: new USB bus registered, assigned bus number 1

isp1362_hc_reset:

 

val=0

 

val=0

 

val=0

Clock not ready after 100ms

isp1362-hcd isp1362-hcd.0: can\'t setup

isp1362-hcd isp1362-hcd.0: USB bus 1 deregistered

init error, -19

 

after i added some debug information

 

I found that  the return value of the function isp1362_read_data16 is always 0

 

I really don\'t know how to solve the problem.

 

//isp1362-hcd.c

 

clkrdy = isp1362_read_reg16(isp1362_hcd, HCuPINT) & HCuPINT_CLKRDY;

 

//isp1362.h

 

 

 

#define isp1362_read_reg16(d, r)        ({            \\

    u16 __v;                            \\

    REG_WIDTH_TEST(ISP1362_REG_##r, REG_WIDTH_16);            \\

    isp1362_write_addr(d, ISP1362_REG_##r);                \\

    __v = isp1362_read_data16(d);                    \\

    RDBG("%s: Read %04x from %s[%02x]\\n", __FUNCTION__, __v, #r,    \\

         ISP1362_REG_NO(ISP1362_REG_##r));                \\

    __v;                                \\

})

 

 

 

static u16 isp1362_read_data16(struct isp1362_hcd *isp1362_hcd)

{

    u16 val;

 

    _BUG_ON(!irqs_disabled());

    DUMMY_DELAY_ACCESS;

    val = readw(isp1362_hcd->data_reg);

 

 

    //printk("val= %d\\n",val);

 

    return val;

}

 

 

 

after I remove the codes:

 

//isp1362-hcd.c

 

//if (!clkrdy) {

        //ERR("Clock not ready after //%lums\\n", timeout);

        //ret = -ENODEV;

    //}

 

 

 

new problem appeared :  Invalid chip ID 0000

 

//isp1362-hcd.c

 

spin_lock_irqsave(&isp1362_hcd->lock, flags);

    chipid = isp1362_read_reg16(isp1362_hcd, HCCHIPID);

    spin_unlock_irqrestore(&isp1362_hcd->lock, flags);

 

    if ((chipid & HCCHIPID_MASK) != HCCHIPID_MAGIC) {

        ERR("%s: Invalid chip ID %04x\\n", __func__, chipid);

        return -ENODEV;

    }

TranslateQuoteReplyEditDelete

 

 

2009-08-10 09:47:43     isp1362_hc_reset: Clock not ready after 100ms

Michael Hennerich (GERMANY)

Message: 78561    Which release are you using?

What is your SCLK and EBIU setting? (kernel config)?

QuoteReplyEditDelete

 

 

2009-08-10 10:15:16     Re: isp1362_hc_reset: Clock not ready after 100ms

Chunbo Fan (CHINA)

Message: 78562   

 

uClinux-dist-2009R1-RC1

 

and sclk is 12M

 

(0x7BB0) Bank 0 (AMBCTL0.L)                                    

(0x7BB0) Bank 1 (AMBCTL0.H)                                   

(0x7BB0) Bank 2 (AMBCTL1.L)                                    

(0xAAC2) Bank 3 (AMBCTL1.H)

TranslateQuoteReplyEditDelete

 

 

2009-08-10 10:31:29     Re: isp1362_hc_reset: Clock not ready after 100ms

Michael Hennerich (GERMANY)

Message: 78563    >and sclk is 12M

 

I assume you meant 120MHz?

What hardware are you using?

I recently tested the ISP1362-hcd driver and it worked ok.

QuoteReplyEditDelete

 

 

2009-08-10 10:34:32     Re: isp1362_hc_reset: Clock not ready after 100ms

Chunbo Fan (CHINA)

Message: 78564   

 

sorry!  the sclk is 27M  and the isp1362 clock is 12M.

TranslateQuoteReplyEditDelete

 

 

2009-08-10 11:20:46     Re: isp1362_hc_reset: Clock not ready after 100ms

Chunbo Fan (CHINA)

Message: 78569   

 

very sorry!! when I reboot the system ,I found that the system clock is 118M and the core clock is 594M.

TranslateQuoteReplyEditDelete

 

 

2009-08-10 11:23:01     Re: isp1362_hc_reset: Clock not ready after 100ms

Michael Hennerich (GERMANY)

Message: 78570    What hardware are you using?

QuoteReplyEditDelete

 

 

2009-08-10 21:20:39     Re: isp1362_hc_reset: Clock not ready after 100ms

Chunbo Fan (CHINA)

Message: 78580   

 

TranslateQuoteReplyEditDelete

 

 

2009-08-11 04:33:05     Re: isp1362_hc_reset: Clock not ready after 100ms

Michael Hennerich (GERMANY)

Message: 78603    Hi Fan,

 

So far you failed to tell me you're Hardware.

I tested the ISP1362-HCD driver on BF533-EZKIT with the Blackfin USB

Extender Card.

 

  docs.blackfin.uclinux.org/doku.php?id=3Dhw:cards:usb_ez-extender

 

See my setup below - I jumpered JP3 to J2-44 for IRQ_PF14.

See config and kernel messages below - it works great.

What you're describing can be caused be two things -=20

1) No hardware present=20

2) You use the wrong base address=20

 

#if defined(CONFIG_USB_ISP1362_HCD) ||

defined(CONFIG_USB_ISP1362_HCD_MODULE)

static struct resource isp1362_hcd_resources[] =3D {

{

.start =3D 0x20360000,

.end =3D 0x20360000,

.flags =3D IORESOURCE_MEM,

}, {

.start =3D 0x20360004,

.end =3D 0x20360004,

.flags =3D IORESOURCE_MEM,

}, {

.start =3D IRQ_PF14,

.end =3D IRQ_PF14,

.flags =3D IORESOURCE_IRQ | IORESOURCE_IRQ_HIGHLEVEL,

},

};

 

static struct isp1362_platform_data isp1362_priv =3D {

.sel15Kres =3D 1,

.clknotstop =3D 0,

.oc_enable =3D 0,

.int_act_high =3D 0,

.int_edge_triggered =3D 0,

.remote_wakeup_connected =3D 0,

.no_power_switching =3D 1,

.power_switching_mode =3D 0,

};

 

static struct platform_device isp1362_hcd_device =3D {

.name =3D "isp1362-hcd",

.id =3D 0,

.dev =3D {

.platform_data =3D &isp1362_priv,

},

.num_resources =3D ARRAY_SIZE(isp1362_hcd_resources),

.resource =3D isp1362_hcd_resources,

};

#endif

 

Linux version 2.6.28.10-ADI-2009R1-svn7130 (michael@mhenneri-D02) (gcc

version 4.1.2 (ADI svn)) #319 Tue Aug 11 10:12:9

bootconsole [early_shadow0] enabled

 

bootconsole [early_BFuart0] enabled

 

early printk enabled on early_BFuart0

 

Board Memory: 32MB

 

Kernel Managed Memory: 32MB

 

Memory map:

 

fixedcode =3D 0x00000400-0x00000490

 

text =3D 0x00001000-0x00112ba0

 

rodata =3D 0x00112ba0-0x00165f88

 

bss =3D 0x00166000-0x00176930

 

data =3D 0x00176930-0x00186000

 

stack =3D 0x00184000-0x00186000

 

init =3D 0x00186000-0x0065d000

 

available =3D 0x0065d000-0x01eff000

 

DMA Zone =3D 0x01f00000-0x02000000

 

Hardware Trace Active and Enabled

 

Boot Mode: 0

 

Blackfin support (C) 2004-2009 Analog Devices, Inc.

 

Compiled for ADSP-BF533 Rev 0.5

 

Blackfin Linux support by   blackfin.uclinux.org/

 

Processor Speed: 594 MHz core clock and 118 MHz System Clock

 

NOMPU: setting up cplb tables

 

Instruction Cache Enabled for CPU0

 

Data Cache Enabled for CPU0 (write-back)

 

Built 1 zonelists in Zone order, mobility grouping off. Total pages:

7873 =20

Kernel command line: bootargs=3Droot=3D/dev/mtdblock0 rw =

clkin_hz=3D27000000

earlyprintk=3Dserial,uart0,57600 console=3DttyBF0,50

Configuring Blackfin Priority Driven Interrupts

 

PID hash table entries: 128 (order: 7, 512 bytes)

 

console handover:boot [early_BFuart0] boot [early_shadow0] -> real

[ttyBF0] =20

Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)

 

Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)

 

Memory available: 24936k/32768k RAM, (4956k init code, 1094k kernel

code, 462k data, 1024k dma, 292k reserved) =20

Calibrating delay loop... 1183.74 BogoMIPS (lpj=3D2367488)

 

Security Framework initialized

 

Mount-cache hash table entries: 512

 

Blackfin Scratchpad data SRAM: 4 KB

 

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

 

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

 

Blackfin L1 Instruction SRAM: 64 KB (52 KB free)

 

net_namespace: 288 bytes

 

NET: Registered protocol family 16

 

Blackfin DMA Controller

 

ezkit_init(): registering device resources

 

usbcore: registered new interface driver usbfs

 

usbcore: registered new interface driver hub

 

usbcore: registered new device driver usb

 

NET: Registered protocol family 2

 

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

 

TCP established hash table entries: 1024 (order: 1, 8192 bytes)

 

TCP bind hash table entries: 1024 (order: 0, 4096 bytes)

 

TCP: Hash tables configured (established 1024 bind 1024)

 

TCP reno registered

 

NET: Registered protocol family 1

 

msgmni has been set to 48

 

io scheduler noop registered

 

io scheduler anticipatory registered (default)

 

io scheduler cfq registered

 

Serial: Blackfin serial driver

 

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq =3D 21) is a BFIN-UART

 

brd: module loaded

 

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version

1.0, regs_base@ffc00500, dma channel@5 =20

driver isp1362-hcd, 2005-04-04

 

isp1362-hcd isp1362-hcd.0: ISP1362 Host Controller

 

isp1362-hcd isp1362-hcd.0: new USB bus registered, assigned bus number 1

 

isp1362_hc_reset:

 

isp1362-hcd isp1362-hcd.0: irq 47, io mem 0x20360000

 

isp1362_hc_start:

 

isp1362-hcd isp1362-hcd.0: ISP1362 Memory usage:

 

isp1362-hcd isp1362-hcd.0: ISTL: 2 * 256: 512 @ $0000:$0100

 

isp1362-hcd isp1362-hcd.0: INTL: 16 * ( 64+8): 1152 @ $0200

 

isp1362-hcd isp1362-hcd.0: ATL : 32 * ( 64+8): 2304 @ $0680

 

isp1362-hcd isp1362-hcd.0: USED/FREE: 3968 128

 

usb usb1: configuration #1 chosen from 1 choice

 

hub 1-0:1.0: USB hub found

 

hub 1-0:1.0: 2 ports detected

 

usb usb1: New USB device found, idVendor=3D1d6b, idProduct=3D0001

 

usb usb1: New USB device strings: Mfr=3D3, Product=3D2, SerialNumber=3D1

 

usb usb1: Product: ISP1362 Host Controller

 

usb usb1: Manufacturer: Linux 2.6.28.10-ADI-2009R1-svn7130 isp1362-hcd

 

usb usb1: SerialNumber: isp1362-hcd.0

 

ISP1362 Host Controller, irq 47

 

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

 

bfin-wdt: initialized: timeout=3D20 sec (nowayout=3D0)

 

TCP cubic registered

 

NET: Registered protocol family 17

 

rtc-bfin rtc-bfin: setting system clock to 1970-01-01 00:00:39 UTC (39)

 

Freeing unused kernel memory: 4956k freed

 

dma_alloc_init: dma_page @ 0x01a20000 - 256 pages at 0x01f00000

 

_____________________________________

 

a8888b. / Welcome to the uClinux distribution \

 

d888888b. / _ _ \

 

8P"YP"Y88 / | | |_| __ __ (TM) |

 

8|o||o|88 _____/ | | _ ____ _ _ \ \/ / |

 

8' .88 \ | | | | _ \| | | | \ / |

 

8`._.' Y8. \ | |__ | | | | | |_| | / \ |

 

d/ `8b. \ \____||_|_| |_|\____|/_/\_\ |

 

dP . Y8b. \ For embedded processors including |

 

d8:' " `::88b \ the Analog Devices Blackfin /

d8" 'Y88b \___________________________________/

:8P ' :888

8a. : _a88P For further information, check out:

._/"Yaa_: .| 88P| -   blackfin.uclinux.org/

\ YP" `| 8P `. -   docs.blackfin.uclinux.org/

/ \.___.d| .' -   www.uclinux.org/

`--..__)8888P`._.' jgs/a:f -   www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.13.4 (2009-08-03 11:06:48 CEST) built-in shell (msh)

Enter 'help' for a list of built-in commands.

 

root:/> usb 1-2: new full speed USB device using isp1362-hcd and address

2

usb 1-2: configuration #1 chosen from 1 choice

usb 1-2: New USB device found, idVendor=3D0781, idProduct=3D5406

usb 1-2: New USB device strings: Mfr=3D1, Product=3D2, SerialNumber=3D3

usb 1-2: Product: U3 Cruzer Micro

usb 1-2: Manufacturer: SanDisk Corporation

usb 1-2: SerialNumber: 0000162443743A6D

QuoteReplyEditDelete

 

 

2009-08-11 07:04:38     Re: isp1362_hc_reset: Clock not ready after 100ms

Chunbo Fan (CHINA)

Message: 78620   

 

hi,Michael

 

very sorry! I have uploaded the Schematic diagram ,but it didn't display on the web page.now I upload again!!

 

DM-KIT-CBBF533-I.pdf

DM-KIT-EXBSSK-BF5xx.pdf

sendpix0.jpg

TranslateQuoteReplyEditDelete

 

 

2009-08-11 07:15:46     Re: isp1362_hc_reset: Clock not ready after 100ms

Chunbo Fan (CHINA)

Message: 78621   

 

hi,

 

      just now ,I check the base address and the hardware , the base address is right and the hardware isp1362 is also

 

present.

TranslateQuoteReplyEditDelete

 

 

2009-08-11 07:21:13     Re: isp1362_hc_reset: Clock not ready after 100ms

Chunbo Fan (CHINA)

Message: 78622   

 

## Booting kernel from Legacy Image at 01000000 ...                            

   Image Name:   Linux-2.6.28.10-ADI-2009R1                                    

   Created:      2009-08-11  10:40:13 UTC                                      

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)                 

   Data Size:    3937824 Bytes =  3.8 MB                                       

   Load Address: 00001000                                                      

   Entry Point:  001e9624                                                      

   Verifying Checksum ... OK                                                   

   Uncompressing Kernel Image ... OK                                           

Starting Kernel at = 001e9624                                                  

Linux version 2.6.28.10-ADI-2009R1 (vs@vs-laptop) (gcc version 4.1.2 (ADI svn))9

bootconsole [early_shadow0] enabled                                            

bootconsole [early_BFuart0] enabled                                            

early printk enabled on early_BFuart0                                          

Warning: limiting memory to 31MB due to hardware anomaly 05000263              

Board Memory: 32MB                                                             

Kernel Managed Memory: 32MB                                                    

Memory map:                                                                    

  fixedcode = 0x00000400-0x00000490                                            

  text      = 0x00001000-0x00151980                                            

  rodata    = 0x00151980-0x001b30a4                                            

  bss       = 0x001b4000-0x001cb828                                            

  data      = 0x001cb840-0x001de000                                            

    stack   = 0x001dc000-0x001de000                                            

  init      = 0x001de000-0x0078e000                                            

  available = 0x0078e000-0x01eff000                                            

  DMA Zone  = 0x01f00000-0x02000000                                            

Hardware Trace Active and Enabled                                              

Boot Mode: 0                                                                   

Blackfin support (C) 2004-2009 Analog Devices, Inc.                            

Compiled for ADSP-BF532 Rev 0.4                                                

Blackfin Linux support by   blackfin.uclinux.org/                         

Processor Speed: 594 MHz core clock and 118 MHz System Clock                   

NOMPU: setting up cplb tables                                                  

Instruction Cache Enabled for CPU0                                             

Data Cache Enabled for CPU0 (write-back)                                       

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 7873     

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=27000000 earlyprintk=seriaf

Configuring Blackfin Priority Driven Interrupts                                

PID hash table entries: 128 (order: 7, 512 bytes)                              

console handover:boot [early_BFuart0] boot [early_shadow0]  -> real [ttyBF0]   

Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)                  

Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)                    

Memory available: 23716k/32768k RAM, (5824k init code, 1346k kernel code, 562k )

Calibrating delay loop... 1183.74 BogoMIPS (lpj=2367488)                       

Security Framework initialized                                                 

Mount-cache hash table entries: 512                                            

Blackfin Scratchpad data SRAM: 4 KB                                            

Blackfin L1 Instruction SRAM: 32 KB (20 KB free)                               

net_namespace: 288 bytes                                                       

NET: Registered protocol family 16                                             

Blackfin DMA Controller                                                        

ezkit_init(): registering device resources                                     

usbcore: registered new interface driver usbfs                                 

usbcore: registered new interface driver hub                                   

usbcore: registered new device driver usb                                      

NET: Registered protocol family 2                                              

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)                 

TCP established hash table entries: 1024 (order: 1, 8192 bytes)                

TCP bind hash table entries: 1024 (order: 0, 4096 bytes)                       

TCP: Hash tables configured (established 1024 bind 1024)                       

TCP reno registered                                                            

NET: Registered protocol family 1                                              

JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.                           

msgmni has been set to 46                                                      

io scheduler noop registered                                                   

io scheduler anticipatory registered (default)                                 

io scheduler cfq registered                                                    

Serial: Blackfin serial driver                                                 

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 21) is a BFIN-UART               

brd: module loaded                                                             

dm9000 Ethernet Driver                                                         

eth0: dm9000 at 20320000,20320010 IRQ 38 MAC: 08:00:3e:26:0a:5b                

Linux video capture interface: v2.00                                           

usbcore: registered new interface driver dabusb                                

dabusb: v1.54:DAB-USB Interface Driver for Linux (c)1999                       

usbcore: registered new interface driver uvcvideo                              

USB Video Class driver (v0.1.0)                                                

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_5

driver isp1362-hcd, 2005-04-04                                                 

isp1362-hcd isp1362-hcd.0: ISP1362 Host Controller                             

isp1362-hcd isp1362-hcd.0: new USB bus registered, assigned bus number 1       

isp1362_hc_reset:                                                              

Clock not ready after 100ms                                                    

isp1362-hcd isp1362-hcd.0: can't setup                                         

isp1362-hcd isp1362-hcd.0: USB bus 1 deregistered                              

init error, -19                                                                

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0                       

bfin-wdt: initialized: timeout=20 sec (nowayout=0)                             

TCP cubic registered                                                           

NET: Registered protocol family 17                                             

rtc-bfin rtc-bfin: setting system clock to 1970-02-06 00:58:30 UTC (3113910)   

eth0: link down                                                                

IP-Config: Complete:                                                           

     device=eth0, addr=192.168.0.15, mask=255.255.255.0, gw=192.168.0.1,       

     host=bf533-ezkit, domain=, nis-domain=(none),                             

     bootserver=192.168.0.2, rootserver=192.168.0.2, rootpath=                 

Freeing unused kernel memory: 5824k freed                                      

dma_alloc_init: dma_page @ 0x001de000 - 256 pages at 0x01f00000                

                           _____________________________________               

        a8888b.           / Welcome to the uClinux distribution \              

       d888888b.         /       _     _                         \             

       8P"YP"Y88        /       | |   |_|     e   th __0:__  lM) in            

k    up|o|, |8810___0M/  bp   s, |  f _ ul__ l-   du\ \pl/  ex   ,            

                                                                      lp   a   

     | |   | |  _ \| | | | \  /        |                                       

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |            

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |            

     dP   .    Y8b.       \   For embedded processors including   |            

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /             

   d8"         'Y88b        \___________________________________/              

  :8P    '      :888                                                           

   8a.   :     _a88P         For further information, check out:               

._/"Yaa_:   .| 88P|            -   blackfin.uclinux.org/                 

\    YP"    `| 8P  `.          -   docs.blackfin.uclinux.org/            

/     \.___.d|    .'           -   www.uclinux.org/                      

`--..__)8888P`._.'  jgs/a:f    -   www.analog.com/blackfin               

                                                                               

Have a lot of fun...                                                           

                                                                               

                                                                               

BusyBox v1.13.4 (2009-08-11 18:38:46 CST) built-in shell (msh)                 

Enter 'help' for a list of built-in commands.         

TranslateQuoteReplyEditDelete

 

 

2009-08-11 08:19:47     Re: isp1362_hc_reset: Clock not ready after 100ms

Michael Hennerich (GERMANY)

Message: 78660    >driver isp1362-hcd, 2005-04-04

>isp1362-hcd isp1362-hcd.0: ISP1362 Host Controller

>isp1362-hcd isp1362-hcd.0: new USB bus registered, assigned bus number

1

>isp1362_hc_reset:

>Clock not ready after 100ms

>isp1362-hcd isp1362-hcd.0: can't setup

>isp1362-hcd isp1362-hcd.0: USB bus 1 deregistered

>init error, -19

 

I get exactly the same thing in case I remove the ISP1362 card from my

EZKIT and then start the kernel.

Your ISP1362_CS chip select is controlled by some glue logic inside the

CPLD on your board - I would start looking there if the ISP1362_CS

really toggles when you access ISP1362 registers.

 

-Michael

QuoteReplyEditDelete

 

 

2009-08-11 09:48:50     Re: isp1362_hc_reset: Clock not ready after 100ms

Chunbo Fan (CHINA)

Message: 78662   

 

OK.It works OK.just because the CS pin didn't toggle.

 

thank you very much  Michael.

 

-Chunbo Fan

TranslateQuoteReplyEditDelete

 

 

2009-12-22 21:11:06     Re: isp1362_hc_reset: Clock not ready after 100ms

fengsheng xiang (CHINA)

Message: 83851   

 

OK.It works OK.just because the CS pin didn't toggle.

 

thank you very much  Michael.

 

-Chunbo Fan

 

---

 

Hi, Chunbo Fan, I'm using the same platform with and  meet the same problem with you.

 

Can you explain the  "CS pin didn't toggle" and how do you solve the problem??

 

Thanks very much,,,

Outcomes