2009-07-30 06:19:58     bfin-linux-uclibc-strip command not found

Document created by Aaronwu Employee on Aug 16, 2013
Version 1Show Document
  • View in full screen mode

2009-07-30 06:19:58     bfin-linux-uclibc-strip command not found

Jithender Golamari (IRELAND)

Message: 78193   

 

Hi

 

I am working on the bf533 STAMP board, and I was following the documentation shown @

 

  docs.blackfin.uclinux.org/doku.php?id=simple_hello_world_application_example

 

    It worked fine upto a step where I have to strip hello, when i gave the command bfin-linux-uclibc-strip hello, result i got is bfin-linux-uclibc-strip: command not found. can you please help, I am not sure if I have to change the PATH. thank you:)

QuoteReplyEditDelete

 

 

2009-07-30 06:21:37     Re: bfin-linux-uclibc-strip command not found

Jithender Golamari (IRELAND)

Message: 78194   

 

Hi

 

I am working on the bf533 STAMP board, and I was following the documentation shown @

 

  docs.blackfin.uclinux.org/doku.php?id=simple_hello_world_application_example

 

    It worked fine upto a step where I have to strip hello, when i gave the command bfin-linux-uclibc-strip hello, result i got is bfin-linux-uclibc-strip: command not found. can you please help, I am not sure if I have to change the PATH. thank you:)

 

Isorry,  forgot to mention I am using SUSE 11.0 as my OS.

 

---

QuoteReplyEditDelete

 

 

2009-07-30 10:04:24     Re: bfin-linux-uclibc-strip command not found

Robin Getz (UNITED STATES)

Message: 78210   

 

Jithender:

 

Where did you install your toolchain from? (and what version are you using?)

 

rgetz@pinky:~> which bfin-linux-uclibc-gcc

/home/rgetz/blackfin/trunk/gcc-4.3-linux-uclibc/bin/bfin-linux-uclibc-gcc

rgetz@pinky:~> ls /home/rgetz/blackfin/trunk/gcc-4.3-linux-uclibc/bin/bfin-linux-uclibc-strip -l

-rwxr-xr-x 2 rgetz users 3131455 2009-06-20 20:37 /home/rgetz/blackfin/trunk/gcc-4.3-linux-uclibc/bin/bfin-linux-uclibc-strip

 

-Robin

QuoteReplyEditDelete

 

 

2009-07-31 07:07:02     Re: bfin-linux-uclibc-strip command not found

Jithender Golamari (IRELAND)

Message: 78249   

 

Hi Robin,

 

 

 

   I installed the toolchain from this website:   blackfin.uclinux.org/gf/project/toolchain/frs/?action=index and the file name is blackfin-toolchain-uclibc-full-08r1.5-14.i386.tar.tar  I gave the PATH as export PATH=/opt/uClinux/bfin-uclinux/bin:/opt/uClinux/bfin-elf/bin:/opt/uClinux/bfin-linux-uclibc/bin:$PATH

 

 

However, wen i gave the command which bfin-linux-uclibc-gcc, it said Which command not found, can you please help me. also do u know if there is any gateway blocking on the bf533 by any chance. thank you

 

 

 

Jithender

QuoteReplyEditDelete

 

 

2009-07-31 07:33:56     Re: bfin-linux-uclibc-strip command not found

Jithender Golamari (IRELAND)

Message: 78250   

 

Hi Robin,

 

 

 

   I installed the toolchain from this website:   blackfin.uclinux.org/gf/project/toolchain/frs/?action=index and the file name is blackfin-toolchain-uclibc-full-08r1.5-14.i386.tar.tar  I gave the PATH as export PATH=/opt/uClinux/bfin-uclinux/bin:/opt/uClinux/bfin-elf/bin:/opt/uClinux/bfin-linux-uclibc/bin:$PATH

 

 

However, wen i gave the command which bfin-linux-uclibc-gcc, it said Which command not found, can you please help me. also do u know if there is any gateway blocking on the bf533 by any chance. thank you

 

 

 

sorry wen i made few changes to the path and gave the command which bfin-linux-uclibc-gcc, it said which: no bfin-linux-uclibc-gcc in (/opt/kde3/bin:/home/lxuser/bin:/usr/local/bin:/usr/bin:sbin/usr/sbin:/bin:usr/bin/X11:usr/X11R6/bin:usr/games:/usr/lib/jvm/jre/bin:/usr/lib/miy:/usr/lib/mit/sbin:/opt/uClinux/bfin-uclinux/bin)

 

 

 

 

 

Jithender

 

---

QuoteReplyEditDelete

 

 

2009-07-31 07:50:33     Re: bfin-linux-uclibc-strip command not found

Robin Getz (UNITED STATES)

Message: 78252   

 

Jithender:

 

Go back and read the install docs:

 

https://docs.blackfin.uclinux.org/doku.php?id=toolchain:installing

 

You are not installing the proper packages.

QuoteReplyEditDelete

 

 

2009-07-31 08:10:00     Re: bfin-linux-uclibc-strip command not found

Jithender Golamari (IRELAND)

Message: 78253   

 

Hi Robin,

 

Thanks for your reply, I had already installed GCC/binutils/gdb package(blackfin-toolchain-08r1.5-14.i386.rpm)  and uClibc packages(blackfin-toolchain-uclibc-default-08r1.5-14.i386) I am sorry but are there any other files that I need to install, I had read through the manual and doesnt seem like anything left to install,  thank you

 

 

 

Jithender

QuoteReplyEditDelete

 

 

2009-07-31 09:44:36     Re: bfin-linux-uclibc-strip command not found

Robin Getz (UNITED STATES)

Message: 78257   

 

Jithender:

 

You said last time you only installed one package (the tarball) - and now it is two (the rpms)

 

Which is the correct answer? mixing rpms and tarballs will not work. only installing one file will not work.

 

Go back and read the docs.

 

-Robin

QuoteReplyEditDelete

Attachments

    Outcomes