2009-07-22 07:30:01     HDD Mount

Document created by Aaronwu Employee on Aug 16, 2013
Version 1Show Document
  • View in full screen mode

2009-07-22 07:30:01     HDD Mount

sree karan (INDIA)

Message: 77862   

 

Hi,

 

 

 

##############################################################################

 

ide: Assuming 50MHz system bus speed for PIO modes; override with idebus=xx

 

ide0: Blackfin generic IDE interface

 

Probing IDE interface ide0...

 

hda: probing with STATUS(0x50) instead of ALTSTATUS(0xaa)

 

hda: HTS541040G9AT00, ATA DISK drive

 

hdb: probing with STATUS(0x50) instead of ALTSTATUS(0xaa)

 

hdb: probing with STATUS(0x51) instead of ALTSTATUS(0xaa)

 

ide0 at 0x20100000-0x20100007,0x20118004 on irq 33

 

hda: max request size: 512KiB

 

hda: Host Protected Area detected.

 

        current capacity is 78140160 sectors (40007 MB)

 

        native  capacity is 185074430006016 sectors (94758108163 MB)

 

hda: task_no_data_intr: status=0x51 { DriveReady SeekComplete Error }

 

hda: task_no_data_intr: error=0x04 { DriveStatusError }

 

ide: failed opcode was: 0x37

 

hda: 78140160 sectors (40007 MB) w/7539KiB Cache, CHS=16383/255/63

 

hda: cache flushes supported

 

hda: hda1 hda2

 

##############################################################################

 

 

 

I am trying to enable HDD driver in uClinux-dist-2008R1.5-RC3 kernel for the BF533 custom hardware.

 

Though I can mount, read from and write to the hard disk, I get some errors (highlighted in the above log).

 

What should be done to overcome those errors?

 

Kindly help.

 

Thanks in advance

 

 

 

Regards,

 

Karan

QuoteReplyEditDelete

 

 

2010-04-17 23:07:32     Re: HDD Mount

steven O (AFGHANISTAN)

Message: 88549   

 

Hi ,

 

    I have the same problem . had you solved it ? and how to solve it ?

QuoteReplyEditDelete

 

 

2010-04-21 11:44:39     Re: HDD Mount

Robin Getz (UNITED STATES)

Message: 88727   

 

Steven:

 

Start a new thread.

 

-robin

Attachments

    Outcomes