2009-07-20 08:01:38     can4linux in 2009R1

Document created by Aaronwu Employee on Aug 16, 2013
Version 1Show Document
  • View in full screen mode

2009-07-20 08:01:38     can4linux in 2009R1

Hugh Lewis (UNITED KINGDOM)

Message: 77721   

 

Has anyone got the can4linux driver running with the 2009R1 branch. I have it working with 2008R1.5-RC3. But I seem to be unable to configure the kernel to run it in 2009R1.

 

I always get

 

"open error 2:/dev/can0: No such file or directory"

 

the difference between 2009R1 and 2008R1.5-RC3 seem to be in core.c

 

the function calls to "class_device_create" have been changed to "device_create".

 

Any ideas as to where I should look for a solution would be much appreciated.

 

Thanks

 

Hugh

QuoteReplyEditDelete

 

 

2009-07-20 22:43:23     Re: can4linux in 2009R1

Sonic Zhang (CHINA)

Message: 77783   

 

Yes, the test suite against CAN driver in 2009R1-RC1 uClinux-dist passes on bf537-stamp and bf548-ezkit.

 

Please run build script under uClinux-dist/testsuites/canbus to have a try.

QuoteReplyEditDelete

Attachments

    Outcomes