2009-07-20 04:23:13     How to test the connector code?

Document created by Aaronwu Employee on Aug 16, 2013
Version 1Show Document
  • View in full screen mode

2009-07-20 04:23:13     How to test the connector code?

ThangarJ P (INDIA)

Message: 77709   

 

Hi ,

 

i want to test the connector test code (linux2.6/Documentation/connector)to confirm the netlink functionality.

 

what are things need to enabled in the make menuconfig to test that example code?

 

please help me to test that code.

 

 

 

Thanks

QuoteReplyEditDelete

 

 

2009-07-20 04:25:16     Re: How to test the connector code?

Mike Frysinger (UNITED STATES)

Message: 77710   

 

there are no config options.  you go in there and run `make`.

QuoteReplyEditDelete

 

 

2009-07-20 05:05:23     Re: How to test the connector code?

ThangarJ P (INDIA)

Message: 77711   

 

hi Mike,

 

In which folder we have to run make ?

 

the file ucon.c has userspace codes.are we need to run this file from userspace?

 

how can make the cn_test.c file?

 

 

 

please clarify the above

 

 

 

Thanks

QuoteReplyEditDelete

 

 

2009-07-20 05:14:58     Re: How to test the connector code?

Mike Frysinger (UNITED STATES)

Message: 77713   

 

cn_test.c is a normal module.  build it like any other.

 

ucon.c is the example userspace app that connects to the example module.

QuoteReplyEditDelete

Attachments

    Outcomes