2009-07-14 01:04:05     2009R1 Release version

Document created by Aaronwu Employee on Aug 16, 2013
Version 1Show Document
  • View in full screen mode

2009-07-14 01:04:05     2009R1 Release version

Sudhakar GN (INDIA)

Message: 77157   

 

Hi ,

 

We plan to build a network player with BF527 DSP  (0.2 Silicon)  and USB (through external USB controller) which will need a official release as a stable base.

 

Could you provide the link to official release version which supports 0.2 Silicon + USB MSC stack as part of kernel. (USB controller is vendor provided)

 

Regarads,

 

Sudhakar

QuoteReplyEditDelete

 

 

2009-07-14 02:22:25     Re: 2009R1 Release version

Yi Li (CHINA)

Message: 77159   

 

Sudhakar,

 

You can either checkout uclinux-dist and linux-kernel from 2009R1 svn branch. Or you can download tar ball from:

 

http://blackfin.uclinux.org/gf/download/frsrelease/380/6527/uClinux-dist-2009R1-RC1.tar.bz2

 

-Yi

QuoteReplyEditDelete

 

 

2009-07-14 02:33:18     Re: 2009R1 Release version

Sudhakar GN (INDIA)

Message: 77160   

 

Thanks for the information.

 

We do not intend to use trunk  and would like to use release branch.

 

Is this official release of 2009R1. Could you please clarify?

QuoteReplyEditDelete

 

 

2009-07-14 02:49:10     Re: 2009R1 Release version

Yi Li (CHINA)

Message: 77161   

 

2009R1 branch is official release - there will be bug fixes, but there is no new features to be added.

QuoteReplyEditDelete

 

 

2009-07-14 19:31:00     Re: 2009R1 Release version

Robin Getz (UNITED STATES)

Message: 77266   

 

Sudhakar:

 

There is no such thing as "official release".

 

Please refer to:

 

https://docs.blackfin.uclinux.org/doku.php?id=processes#releases

 

The only "official" release is the fixes that have been commited to the branch.

 

-Robin

QuoteReplyEditDelete

 

 

2009-07-15 06:01:06     Re: 2009R1 Release version

Sudhakar GN (INDIA)

Message: 77332   

 

Got it. Thanks Robin!

Attachments

    Outcomes