2009-07-10 06:50:30     ftp error for my sda

Document created by Aaronwu Employee on Aug 16, 2013
Version 1Show Document
  • View in full screen mode

2009-07-10 06:50:30     ftp error for my sda

billy zhou (UNITED STATES)

Message: 77034   

 

Now I use my sata work normally, read/write correctly.

 

But when I use ftpd as ftp server, and use filezilla as ftp client, it get error if I try to cd my sda.

 

 

 

my sda info:

 

scsi0 : pata_platform

ata1: PATA max PIO0 no IRQ, using PIO polling mmio cmd 0x20200020 ctl 0x2020001c

ata1.00: ATA-8: Hitachi HTS543216L9A300, FB2OC40C, max UDMA/133

ata1.00: 312581808 sectors, multi 0: LBA48 NCQ (depth 0/1)

ata1.00: configured for PIO

scsi 0:0:0:0: Direct-Access     ATA      Hitachi HTS54321 FB2O PQ: 0 ANSI: 5

sd 0:0:0:0: [sda] 312581808 512-byte hardware sectors: (160 GB/149 GiB)

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA

sd 0:0:0:0: [sda] 312581808 512-byte hardware sectors: (160 GB/149 GiB)

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA

sda: unknown partition table

sd 0:0:0:0: [sda] Attached SCSI disk

sd 0:0:0:0: Attached scsi generic sg0 type 0

 

 

 

 

 

root:/usr/local> mount

rootfs on / type rootfs (rw)

/dev/root on / type ext2 (rw)

proc on /proc type proc (rw)

ramfs on /var type ramfs (rw)

sysfs on /sys type sysfs (rw)

devpts on /dev/pts type devpts (rw,mode=600)

/dev/sda on /usr/local type ext3 (rw,errors=continue,data=ordered)

root:/usr/local> ls

lost+found  rc

root:/usr/local> df

Filesystem           1K-blocks      Used Available Use% Mounted on

/dev/root                 7163      1378      5785  19% /

/dev/sda             155059068    192076 147052448   0% /usr/local

root:/usr/local> cp /etc/hosts ./

status check failed: 129                                   (this line seems error!)

root:/usr/local> ls

hosts       lost+found  rc

root:/usr/local>

 

 

 

my filezilla error info:

 

状态:    读取目录列表...

命令:    CWD /usr

返回:    250 CWD command successful.

命令:    PASV

返回:    227 Entering Passive Mode (192,168,2,222,177,234)

命令:    LIST

返回:    150 Opening BINARY mode data connection for '/bin/ls'.

返回:    226 Transfer complete.

状态:    列目录成功

状态:    读取目录列表...

命令:    CWD /usr/local

返回:    250 CWD command successful.

命令:    PASV

返回:    227 Entering Passive Mode (192,168,2,222,226,30)

命令:    LIST

返回:    550 /bin/ls: Illegal seek.

错误:    读取目录列表失败

QuoteReplyEditDelete

 

 

2009-07-10 09:55:45     Re: ftp error for my sda

Mike Frysinger (UNITED STATES)

Message: 77037   

 

so look at the ftpd debug logs and make sure your ftpd has permission to read /usr/local

Attachments

    Outcomes