2009-06-11 08:12:18     probleam in ping with remote network

Document created by Aaronwu Employee on Aug 15, 2013
Version 1Show Document
  • View in full screen mode

2009-06-11 08:12:18     probleam in ping with remote network

roopesh motewar (INDIA)

Message: 75533   

 

HI

 

WE build the ip04 successfully. now we are using it with

our application.

i am facing strange problem with networking.

with normal set up i am able to ping any www.XXX.com web site.

but when we put the ip04 in our customer network the ip04

is not able to ping.

the network connections are as follows

ip04<---->cisco(L2) switch<---->cisco(L3)

switch<----->cisco core router(CISCO690X)<---

-->DWPM<------->DWPM<--->cisco core router(CISCO690X)<--->cisco(L3)

switch<------->cisco(L2) switch<------->PC1

presently our providing us voice VLAN port

PC1 and ip04 both are having static IP, but ping is failed from both the side.

for testing the port if i replaced ip04 with PC2 or IP PHONE(snom) the

ping is successful.

i thing it is due to netfilter.

 

presently i am not able to understand where the things are wrong.

can you help me out to solve this problem

 

 

Thanks

 

Roop

QuoteReplyEditDelete

 

 

2009-06-11 08:18:23     Re: probleam in ping with remote network

Mike Frysinger (UNITED STATES)

Message: 75535   

 

the ip04 board is supported in the asterisk forums:

  blackfin.uclinux.org/gf/project/asterisk/

Attachments

    Outcomes