2009-06-02 05:25:46     Setup tftp beginners Questions

Document created by Aaronwu Employee on Aug 15, 2013
Version 1Show Document
  • View in full screen mode

2009-06-02 05:25:46     Setup tftp beginners Questions

Raphael Lang (GERMANY)

Message: 75008   

 

Hello Dear ucLinux People

 

I just want to start with Blackfin uclinux and i installed all the toolchain and the U-Boot

 

I got some problems to setup the TFTP server.

 

I did everything like on the description on  http://docs.blackfin.uclinux.org/doku.php?id=setting_up_a_tftp_server

 

instead:

 

Create /etc/xinetd.d/tftp and put this entry:

 

service tftp

{

protocol        = udp

socket_type     = dgram

wait            = yes

user            = root

server          = /usr/sbin/in.tftpd

server_args     = -s /tftpboot

disable         = no

}

 

Must i creat a new file with the name tftp with that entry ? What ist the ending of the file tftp.* ?

 

How to created a file in that direction because I am not able to do that, ubuntu tells me : permission denied

 

must I change the root rights or use special command. Sorry I am new on Linux but I want to learn

 

thanks for help

 

Rapheal

TranslateQuoteReplyEditDelete

 

 

2009-06-02 05:34:13     Re: Setup tftp beginners Questions

Mike Frysinger (UNITED STATES)

Message: 75009   

 

setup needs to be done as root or by using sudo.  non root users never have write access to anything in /etc/.

 

QuoteReplyEditDelete

 

 

2009-06-02 06:16:30     Re: Setup tftp beginners Questions

Raphael Lang (GERMANY)

Message: 75011   

 

ok, how to create that new file ?

 

which command i need ?

TranslateQuoteReplyEditDelete

 

 

2009-06-02 06:21:00     Re: Setup tftp beginners Questions

Mike Frysinger (UNITED STATES)

Message: 75014   

 

use any text editor

QuoteReplyEditDelete

 

 

2009-06-03 04:20:27     Re: Setup tftp beginners Questions

Raphael Lang (GERMANY)

Message: 75076   

 

Ok thanks, it worked

TranslateQuoteReplyEditDelete

Attachments

    Outcomes