2009-05-25 08:34:32     reboot command from kernel

Document created by Aaronwu Employee on Aug 15, 2013
Version 1Show Document
  • View in full screen mode

2009-05-25 08:34:32     reboot command from kernel

Servaes Joordens (NETHERLANDS)

Message: 74537   

 

How can I call a reboot command from within the kernel? I want to have the same effect as if I typed reboot from the command-line.

QuoteReplyEditDelete

 

 

2009-05-25 09:08:20     reboot command from kernel

Michael Hennerich (GERMANY)

Message: 74541    You should use kernel_restart, kernel_halt, kernel_power_off these will

map to

arch/blackfin/kernel/reboot.c machine_restart() and friends.

 

Better - You should also have a look at:

native_machine_restart() in arch/blackfin/mach-bf537/boards/stamp.

 

You need to add something similar to address your gpio issue on your

board.

 

-Michael

QuoteReplyEditDelete

 

 

2009-05-25 10:47:18     Re: reboot command from kernel

Servaes Joordens (NETHERLANDS)

Message: 74542   

 

thanks, I will try it

Attachments

    Outcomes