2009-05-21 10:54:52     ISP1362 as peripheral

Document created by Aaronwu Employee on Aug 15, 2013
Version 1Show Document
  • View in full screen mode

2009-05-21 10:54:52     ISP1362 as peripheral

xabi romero (UNITED STATES)

Message: 74416   

 

Hi to everybody.

 

I am working with the Bluetechnix CM-BF561V2 and the DEv-Board V2.2. In this board, the USB chip is the ISP1362. It works fine as host, but i am trynig to work like a peripheral, because i need to communicate with a PC using gadget serial.(Linux gadget serial driver)

 

Is it possible? the last release of the uclinux supports the peripheral (or OTG) class with the ISP1362?

 

Thanks to everybody

QuoteReplyEditDelete

 

 

2009-05-22 18:21:56     Re: ISP1362 as peripheral

Steve Strobel (UNITED STATES)

Message: 74463   

 

I asked a similar question here:

 

  blackfin.uclinux.org/gf/project/uclinux-dist/forum/?_forum_action=ForumMessageBrowse&thread_id=24167&action=ForumBrowse&forum_id=39

 

(or if the long URL gives you trouble):

 

  tinyurl.com/qrctrv

 

Steve

QuoteReplyEditDelete

 

 

2009-05-23 04:15:39     Re: ISP1362 as peripheral

xabi romero (UNITED STATES)

Message: 74469   

 

Ok. Thak you very much for your answer.

 

Do you do anythig with the ISB1362 to work as device? or finally , you had changed the device.

 

Thanks againn.

 

XaBi

QuoteReplyEditDelete

 

 

2009-05-26 13:37:21     Re: ISP1362 as peripheral

Steve Strobel (UNITED STATES)

Message: 74618   

 

> Do you do anythig with the ISB1362 to work as device? or finally , you had changed the device.

 

We are using only host mode and hoping that someone else will write the device-mode driver

 

Steve

Attachments

    Outcomes