2009-04-21 07:12:38     zeroconf

Document created by Aaronwu Employee on Aug 15, 2013
Version 1Show Document
  • View in full screen mode

2009-04-21 07:12:38     zeroconf

Daniele Pagani (ITALY)

Message: 72938   

 

Dear sirs,

 

could somebody suggest me an application in order to run zeroconf protocol, or Bonjour or something similar in order to have the network autoconfiguration?

 

I've found the zcip under the BusyBox menu. Does exist something more?

 

This application needs to run on Blackfin BF537 and on Pc Windows machine (of course not the same application, but the same protocol).

 

Best regards,

 

Daniele.

TranslateQuoteReplyEditDelete

 

 

2009-04-21 07:33:42     Re: zeroconf

Robin Getz (UNITED STATES)

Message: 72972   

 

Daniele:

 

Have a look at avahi. It is already in the uClinux-dist. (./lib/avahi/)

 

-Robin

QuoteReplyEditDelete

 

 

2009-04-21 08:55:21     Re: zeroconf

Daniele Pagani (ITALY)

Message: 72988   

 

Dear Robin,

 

I'm using live distribution rev 7972.

 

I've find avahi in lib. If I compile, than I've:

 

libavahi-common.so.3 and libavahi-core.so.5 in /usr/lib directory, but I don't find any avahi application.

 

Do I write my application using this library? or is there a ready application?

 

Regards,

 

Daniele.

TranslateQuoteReplyEditDelete

 

 

2009-04-21 11:50:56     Re: zeroconf

Robin Getz (UNITED STATES)

Message: 73002   

 

Daniele:

 

Have a look at the docs:

 

  avahi.org/

 

Normally - people use their own - but I think there are likely some things in ./staging that aren't installed into the romfs.

 

  avahi.org/wiki/Avah4users#Documentation

 

-Robin

Attachments

    Outcomes