2009-04-07 05:17:57     use the rs232 port

Document created by Aaronwu Employee on Aug 14, 2013
Version 1Show Document
  • View in full screen mode

2009-04-07 05:17:57     use the rs232 port

Amine Salmen Rekik (TUNISIA)

Message: 72307   

 

hello

 

can i  use the uart port of my stamp (BF548)? indeed i have to connect a medical device to the stamp and send its data to a remote server using Ip network. my problem is that the uart port is used to communicate with the pc so i should close this connection and init another one with my device but i don't arrive.

QuoteReplyEditDelete

 

 

2009-04-07 05:22:17     Re: use the rs232 port

Mike Frysinger (UNITED STATES)

Message: 72309   

 

you can use the UARTs however you want.  if you dont want a console running on a UART, then dont configure it that way.

 

docs.blackfin.uclinux.org/doku.php?id=silent_booting#linux_kernel

QuoteReplyEditDelete

 

 

2009-04-07 07:00:18     Re: use the rs232 port

Amine Salmen Rekik (TUNISIA)

Message: 72319   

 

hello,

 

Do you have an example that shows how can i configure the uart port in my board and how can i send and receive data.

 

thank you very well

 

 

 

 

QuoteReplyEditDelete

 

 

2009-04-07 15:01:43     Re: use the rs232 port

Mike Frysinger (UNITED STATES)

Message: 72343   

 

https://docs.blackfin.uclinux.org/doku.php?id=uclinux-dist:serial_programming

Attachments

    Outcomes