2009-04-03 09:28:51     No u-boot-1.1.6 (or any VER)

Document created by Aaronwu Employee on Aug 14, 2013
Version 1Show Document
  • View in full screen mode

2009-04-03 09:28:51     No u-boot-1.1.6 (or any VER)

Jim Carstensen (UNITED STATES)

Message: 72111   

 

Using this document:

 

https://docs.blackfin.uclinux.org/doku.php?id=developing_with_blackfin_live_sources

 

Checked out everything (NOT behind firewall).

 

Built toolchain - all normal.

 

Set Path - all normal ( verified usng procedure, etc.)

 

Now get to the point where I want to build u-boot.

 

"Working in the u-boot source is the same as any release. Just use the directory ~/blackfin-sources/u-boot/u-boot-VER/ (where the exact VER changes over time) and follow the directions in the compiling page. "

 

Problem is that there is no ~/blackfin-sources/u-boot/u-boot-VER directory (not u-boot-1.1.6 or any version as described on compiling page).

 

What happened?

 

Thanks.

 

 

 

 

QuoteReplyEditDelete

 

 

2009-04-03 09:32:28     Re: No u-boot-1.1.6 (or any VER)

Mike Frysinger (UNITED STATES)

Message: 72112   

 

why dont you post a listing of what is actually in the directory.  i see plenty of u-boot versions in svn trunk.

 

$ svn ls svn://blackfin.uclinux.org/u-boot/trunk

BUILD-RELEASE

u-boot-1.1.6/

u-boot-2008.10/

u-boot-2009.01/

u-boot-2009.03/

u-boot_test_script/

QuoteReplyEditDelete

 

 

2009-04-03 09:43:13     Re: No u-boot-1.1.6 (or any VER)

Jim Carstensen (UNITED STATES)

Message: 72113   

 

CHANGELOG                                         doc                               lib_ppc

CHANGELOG-before-U-Boot-1.1.5   drivers                          localversion-adi

COPYING                                                dtt                                  m68k_config.mk

CREDITS                                                examples                    microblaze_config.mk

MAINTAINERS                                       fs                                  mips_config.mk

MAKEALL                                                i386_config.mk         mkconfig

Makefile                                                   include                        nand_spl

README                                                 lib_arm                       net

arm_config.mk                                       lib_avr32                     nios2_config.mk

avr32_config.mk                                    lib_blackfin                 nios_config.mk

blackfin_config.mk                                lib_generic                 patches

board                                                       lib_i386                       post

common                                                 lib_m68k                     ppc_config.mk

config.mk                                                lib_microblaze           rtc

cpu                                                           lib_mips                     rules.mk

dir.log                                                      lib_nios                       tools

disk                                                         lib_nios2

uclinux@colinux:~/blackfin-sources/u-boot$

 

QuoteReplyEditDelete

 

 

2009-04-03 09:53:09     Re: No u-boot-1.1.6 (or any VER)

Mike Frysinger (UNITED STATES)

Message: 72114   

 

looks like you didnt delete your old checkout before running the new svn command.  that is trunk/u-boot-1.1.6/.

QuoteReplyEditDelete

 

 

2009-04-03 09:56:47     Re: No u-boot-1.1.6 (or any VER)

Jim Carstensen (UNITED STATES)

Message: 72115   

 

OK.  (as you can probably tell) I'm a relative newbie to this.

 

Could you please tell me how to "delete my old checkout"

 

thanks.

QuoteReplyEditDelete

 

 

2009-04-03 10:31:26     Re: No u-boot-1.1.6 (or any VER)

Mike Frysinger (UNITED STATES)

Message: 72117   

 

`rm -rf` ?

QuoteReplyEditDelete

 

 

2009-04-03 11:17:38     Re: No u-boot-1.1.6 (or any VER)

Jim Carstensen (UNITED STATES)

Message: 72124   

 

hmmm...

 

I did the 'rm -rf' before this and started with a clean slate.  After that, I did this:

 

$ cd ~/blackfin-sources

$ svn checkout svn://blackfin.uclinux.org/toolchain/trunk toolchain

$ svn checkout svn://blackfin.uclinux.org/u-boot/trunk u-boot

$ svn checkout svn://blackfin.uclinux.org/uclinux-dist/trunk uclinux-dist

 

 

also did a 'svn up' in the u-boot directory (and the other two, as well).

 

Is it possible that I need to check it out separately?  Is svn not grabbing the 1.1.6 directory under u-boot?

 

 

QuoteReplyEditDelete

 

 

2009-04-03 11:27:00     Re: No u-boot-1.1.6 (or any VER)

Mike Frysinger (UNITED STATES)

Message: 72126   

 

are you sure that's what you did ?  maybe you were reading an older version of the doc which said to check out u-boot-1.1.6 specifically.

QuoteReplyEditDelete

 

 

2009-04-03 11:39:09     Re: No u-boot-1.1.6 (or any VER)

Jim Carstensen (UNITED STATES)

Message: 72127   

 

Yeah.  I had used the older version of the doc.  And I do remember checking it out separately.  Unfortunately, I was logged in as root and there were some permission issues so I started over (rm -rf).

 

Will there be any problem with the u-boot build if I just go ahead and check it out from the trunk separately?

QuoteReplyEditDelete

 

 

2009-04-03 11:46:38     Re: No u-boot-1.1.6 (or any VER)

Mike Frysinger (UNITED STATES)

Message: 72128   

 

u-boot doesnt care where/how you check it out

QuoteReplyEditDelete

 

 

2009-04-03 12:01:19     Re: No u-boot-1.1.6 (or any VER)

Jim Carstensen (UNITED STATES)

Message: 72129   

 

So just a one more little nudge here...

 

svn checkout svn://blackfin.uclinux.org/u-boot/u-boot-1.1.6/trunk u-boot/u-boot-1.1.6

 

says 'svn://blackfin.uclinux.org/u-boot/u-boot-1.1.6/trunk' doesn't exist.

 

must be typing something wrong?

QuoteReplyEditDelete

 

 

2009-04-03 12:09:53     Re: No u-boot-1.1.6 (or any VER)

Mike Frysinger (UNITED STATES)

Message: 72131   

 

you can click the SVN tab on the left to see the actual layout of svn.  things are in trunk, not the other way around.

QuoteReplyEditDelete

 

 

2009-04-03 12:16:07     Re: No u-boot-1.1.6 (or any VER)

Jim Carstensen (UNITED STATES)

Message: 72132   

 

That's what I thought.  Except the doc shows this...

 

svn checkout svn://blackfin.uclinux.org/u-boot/trunk u-boot

 

 

where the 'trunk' comes last, not before the 'u-boot' so I thought I would follow the same convention.

 

So for this case it's 'trunk/u-boot/u-boot-1.1.6'?

 

I don't see u-boot in the trunk index in the svn tab on the left, here.

 

 

QuoteReplyEditDelete

 

 

2009-04-03 12:36:45     Re: No u-boot-1.1.6 (or any VER)

Mike Frysinger (UNITED STATES)

Message: 72133   

 

that isnt how it works.  you're confusing the forms.  the template is:

svn://<host>/<repository name>/<svn branch>/<random subdir>

 

in this case, the repo is "u-boot", the branch is "trunk", and then you can check out any random subdir you want

QuoteReplyEditDelete

 

 

2009-04-03 14:17:55     Re: No u-boot-1.1.6 (or any VER)

Jim Carstensen (UNITED STATES)

Message: 72136   

 

Ahhhh...I got it.

 

It's downloading now.

 

Thanks.

Attachments

    Outcomes