2009-03-31 15:29:04     increasing size /dev/ram

Document created by Aaronwu Employee on Aug 14, 2013
Version 1Show Document
  • View in full screen mode

2009-03-31 15:29:04     increasing size /dev/ram

Joao Paulo Bodanese (BRAZIL)

Message: 71899   

 

Hi,

 

How can i increase the size of /dev/ram?

 

/home # df

Filesystem 1k-blocks Used Available Use%

/dev/ram 5653 5156 209 96% /

 

I have availiable just 209 bytes ;/

i can't download anything to the board

 

Regards,

João Paulo

QuoteReplyEditDelete

 

 

2009-03-31 15:31:34     Re: increasing size /dev/ram

Mike Frysinger (UNITED STATES)

Message: 71900   

 

so use /var or something else that is mounted as ramfs

 

or read the documentation:

docs.blackfin.uclinux.org/doku.php?id=root_file_system_structure

Attachments

    Outcomes