2009-03-25 02:22:25     Page Allocation failure

Document created by Aaronwu Employee on Aug 14, 2013
Version 1Show Document
  • View in full screen mode

2009-03-25 02:22:25     Page Allocation failure

vijai ragavan (INDIA)

Message: 71481   

 

Dear All,

 

I am using 2008R1.5 distribution for the BF561 processor.

 

I am facing the following issue while exicuting the application on the teraterm.So please suggest how to solve this issue?

 

 

 

 

 

root:/> NetFrame: page allocation failure. order:13, mode:0x40d0

Hardware Trace:

   0 Target : <0x002032a4> { _dump_stack + 0x0 }

     Source : <0x0022434c> { ___alloc_pages + 0x1c8 }

   1 Target : <0x0022434c> { ___alloc_pages + 0x1c8 }

     Source : <0x0020ab2e> { _printk + 0x16 }

   2 Target : <0x0020ab2a> { _printk + 0x12 }

     Source : <0x0020ab16> { _vprintk + 0x2b2 }

   3 Target : <0x0020ab0a> { _vprintk + 0x2a6 }

     Source : <0x0020aae4> { _vprintk + 0x280 }

   4 Target : <0x0020aae4> { _vprintk + 0x280 }

     Source : <0xffa00cd0> { __common_int_entry + 0xd8 }

   5 Target : <0xffa00c6e> { __common_int_entry + 0x76 }

     Source : <0xffa00aa0> { _return_from_int + 0x58 }

   6 Target : <0xffa00aa0> { _return_from_int + 0x58 }

     Source : <0xffa00a76> { _return_from_int + 0x2e }

   7 Target : <0xffa00a48> { _return_from_int + 0x0 }

     Source : <0xffa00c6a> { __common_int_entry + 0x72 }

   8 Target : <0xffa00c68> { __common_int_entry + 0x70 }

     Source : <0xffa003cc> { _asm_do_IRQ + 0x7c }

   9 Target : <0xffa003bc> { _asm_do_IRQ + 0x6c }

     Source : <0x0020e552> { __local_bh_enable + 0xae }

  10 Target : <0x0020e53a> { __local_bh_enable + 0x96 }

     Source : <0x0020e500> { __local_bh_enable + 0x5c }

  11 Target : <0x0020e4f8> { __local_bh_enable + 0x54 }

     Source : <0x0020e4be> { __local_bh_enable + 0x1a }

  12 Target : <0x0020e4a4> { __local_bh_enable + 0x0 }

     Source : <0x0020e5ee> { ___do_softirq + 0x9a }

  13 Target : <0x0020e5e8> { ___do_softirq + 0x94 }

     Source : <0x0020e5c6> { ___do_softirq + 0x72 }

  14 Target : <0x0020e5b8> { ___do_softirq + 0x64 }

     Source : <0x0020e5b2> { ___do_softirq + 0x5e }

  15 Target : <0x0020e5a2> { ___do_softirq + 0x4e }

     Source : <0x00210556> { _run_timer_softirq + 0x152 }

Stack from 00dadc9c:

        0022430a 00224350 00000000 00000000 000040d0 0076e22c 0000000d 000040d0

        000240d0 00000010 00000000 00000000 00224382 0076b840 03b95bc0 00aa22a0

        ffffffda 00000077 00001873 0129b000 0022981c 00000000 00000000 002298f2

        00dac000 00771040 00dadd80 00dadd14 00001802 0129b63f 001fc000 00000000

        00a1a120 0024d9c8 00a1a134 00771074 00a1a128 00000000 00000fff 00000c04

        00001802 00771ba0 0022ffa4 0129a640 00000003 00001802 000001fb 00aa2240

 

Call Trace:

[<00360600>] ___alloc_bootmem_core+0x70/0x2b0

[<0024df5c>] _load_elf_fdpic_binary+0x250/0x9c4

[<003606b8>] ___alloc_bootmem_core+0x128/0x2b0

[<003606b4>] ___alloc_bootmem_core+0x124/0x2b0

[<00200034>] _init_post+0x1c/0xc0

[<00280004>] _cfq_set_request+0x4/0x288

[<002b4970>] _hid_parser_local+0xd8/0xec

[<00200034>] _init_post+0x1c/0xc0

[<00280007>] _cfq_set_request+0x7/0x288

[<0022f5be>] _search_binary_handler+0x32/0xc8

[<003606b8>] ___alloc_bootmem_core+0x128/0x2b0

[<003606b4>] ___alloc_bootmem_core+0x124/0x2b0

[<002307a4>] _do_execve+0xe4/0x198

[<00360664>] ___alloc_bootmem_core+0xd4/0x2b0

[<003606b8>] ___alloc_bootmem_core+0x128/0x2b0

[<00360664>] ___alloc_bootmem_core+0xd4/0x2b0

[<0022b7ce>] _filp_close+0x46/0x58

[<0020073a>] _sys_execve+0x2e/0x4c

[<0020070c>] _sys_execve+0x0/0x4c

[<00360684>] ___alloc_bootmem_core+0xf4/0x2b0

[<003606b4>] ___alloc_bootmem_core+0x124/0x2b0

[<00360684>] ___alloc_bootmem_core+0xf4/0x2b0

[<0036062c>] ___alloc_bootmem_core+0x9c/0x2b0

[<003606b8>] ___alloc_bootmem_core+0x128/0x2b0

[<0036068f>] ___alloc_bootmem_core+0xff/0x2b0

[<00360684>] ___alloc_bootmem_core+0xf4/0x2b0

[<003606b4>] ___alloc_bootmem_core+0x124/0x2b0

[<00360664>] ___alloc_bootmem_core+0xd4/0x2b0

[<003606b8>] ___alloc_bootmem_core+0x128/0x2b0

 

Mem-info:

DMA per-cpu:

CPU    0: Hot: hi:   18, btch:   3 usd:   5   Cold: hi:    6, btch:   1 usd:   0

Active:1206 inactive:1122 dirty:0 writeback:0 unstable:0

free:10428 slab:549 mapped:0 pagetables:0 bounce:0

DMA free:41712kB min:984kB low:1228kB high:1476kB active:4824kB inactive:4488kB present:60960kB pages_scanned:9591 all_unre

claimable? no

lowmem_reserve[]: 0 0

DMA: 0*4kB 2*8kB 0*16kB 1*32kB 1*64kB 1*128kB 0*256kB 1*512kB 0*1024kB 0*2048kB 0*4096kB 1*8192kB 2*16384kB 0*32768kB = 417

12kB

15359 pages of RAM

10456 free pages

1016 reserved pages

1 pages shared

0 pages swap cached

Allocation of length 19509248 from process 54 failed

DMA per-cpu:

CPU    0: Hot: hi:   18, btch:   3 usd:   5   Cold: hi:    6, btch:   1 usd:   0

Active:1206 inactive:1122 dirty:0 writeback:0 unstable:0

free:10428 slab:549 mapped:0 pagetables:0 bounce:0

DMA free:41712kB min:984kB low:1228kB high:1476kB active:4824kB inactive:4488kB present:60960kB pages_scanned:9591 all_unre

claimable? no

lowmem_reserve[]: 0 0

DMA: 0*4kB 2*8kB 0*16kB 1*32kB 1*64kB 1*128kB 0*256kB 1*512kB 0*1024kB 0*2048kB 0*4096kB 1*8192kB 2*16384kB 0*32768kB = 417

12kB

Unable to load executable

 

 

 

 

QuoteReplyEditDelete

 

 

2009-03-25 02:46:06     Re: Page Allocation failure

Mike Frysinger (UNITED STATES)

Message: 71483   

 

your memory is fragmented and doesnt have a 32meg contiguous region.  do all large allocations at first boot and do not free the memory.

QuoteReplyEditDelete

 

 

2009-03-25 02:59:00     Re: Page Allocation failure

vijai ragavan (INDIA)

Message: 71485   

 

Dear Mike,

 

Please tell where i have to modify it?

QuoteReplyEditDelete

 

 

2009-03-25 08:02:20     Re: Page Allocation failure

Robin Getz (UNITED STATES)

Message: 71522   

 

Vijai:

 

Your application is too big - either make it smaller - or add more memory to your system.

 

-Robin

Attachments

    Outcomes