2009-03-18 09:05:14     boa error

Document created by Aaronwu Employee on Aug 14, 2013
Version 1Show Document
  • View in full screen mode

2009-03-18 09:05:14     boa error

Daniele Pagani (ITALY)

Message: 71205   

 

Dear sirs,

 

I've this problem:

 

INFO: task boa:44 blocked for more than 120 seconds.

"echo 0 > /proc/sys/kernel/hung_task_timeout_secs" disables this message.

boa           D ffa008c0     0    44      1

Stack info:

SP: [0x004eddbc] <0x004eddbc> /* kernel dynamic memory */

FP: (0x004eddd8)

Memory from 0x004eddb0 to 004ee000

004eddb0: 004edeac  0055bc6c  0015d46c [007a9c60] 00775380  0055bc40  007a9960

0015d46c

004eddd0: 00000002  004ec000 (004eddf4)<ffa0125a><0003be40> 00000000  004ede10

004ec000

 

004eddf0: 004ec000 (004ede6c)<0010b314> 004ec000  004ec000  004edeac  7fffffff

00000000

004ede10: 00000002  0016add0  003d08ba  004ede48  004ede48  004ede44 <0010b0f8>

001a59a0

004ede30: 7fffffff  00000000  00000000 <0010b180> 004ec000  7fffffff  00000000

004ede80

004ede50:<0000cdac> 0015d46c  00000001  00775380  0000a194  004edeb0  004edeb0 (

00000000)

004ede70:<0000e1cc> 001a59a0  00000000  00000000  00004111  00000000  0000002d

00004000

004ede90: 00000124  002dfdb8  004edf24  00000000  00000000  00000000  00000000

00000000

 

004edeb0: 004ede64  004ede64  002e1880  002dfdd8 <00001634> ffa000e0  000000be

002e1880

004eded0: 00000000  ffffe000  002e3a64  002dfeb4  00000140  00000001  00000000

00000000

004edef0: 00000000  00000000 <ffa000ec> 00000000  ffffe000  00000000 <ffa007fc>

002df800

004edf10: 002e1880  00278b70  00000002  002dfeb4  002e3a64  001cc0ce  00008000

00000000

004edf30: 00000000  004ee000  001cc0ce  001cc0ce <002a4b1a><ffa00d64> 02001025

002a6a4b

004edf50: 007b6361  002a6a4a  007b6354  00000000  00000000  00000006  00000000

00000006

004edf70: 00000000  00000000  00000000  00000000  00000000  00000000  00000000

00000000

004edf90: 00000000  00000000  00000000  00000000  00000000  00000000  00000000

 

002e1880

004edfb0: 002ae430  002dfdb8  002dfdd8  0027cb38  002dfeb4  002e1880  00271408

001cc0c8

004edfd0: 000000be  00000003  00000003  002e3a64  002dfeb4  00000002  00000001

7fffffff

004edff0: 00000001  00000001  000000be  00000006  004eb0e0

Return addresses in stack:

   frame  1 : <0xffa0125a> { _schedule + 0x182 }

    address : <0x0003be40> { _kmem_cache_alloc + 0x54 }

   frame  2 : <0x0010b314> { _schedule_timeout + 0x6c }

    address : <0x0010b0f8> { __cond_resched + 0x34 }

    address : <0x0010b180> { _wait_for_common + 0x84 }

    address : <0x0000cdac> { _wake_up_new_task + 0x84 }

   frame  3 : <0x0000e1cc> { _do_fork + 0xd8 }

    address : <0x00001634> { _bfin_vfork + 0x18 }

    address : <0xffa000ec> { _sys_vfork + 0xc }

    address : <0xffa007fc> { _system_call + 0x68 }

    address : <0x002a4b1a> [ /bin/boa + 0x4b1a ]

    address : <0xffa00d64> { _evt_system_call + 0x64 }

 

I've started boa with boa -f /etc/boa.conf &

 

BF537

 

uclinux-dist revision 7862

 

linux revision 6164

 

Regards,

 

Daniele.

 

 

 

 

TranslateQuoteReplyEditDelete

 

 

2009-03-20 21:58:40     Re: boa error

Robin Getz (UNITED STATES)

Message: 71323   

 

Daniele:

 

What type of html/script is boa pointing to?

 

 

QuoteReplyEditDelete

 

 

2009-03-24 04:56:01     Re: boa error

Daniele Pagani (ITALY)

Message: 71431   

 

Dear Robin,

 

the config file for boa is the same as the original; according to

 

docs.blackfin.uclinux.org/doku.php?id=uclinux-dist:boa

 

I've changed the cgi line (in order to use cgi)

 

Then, the site has some standard html files and some cgi.

 

With cgi I do something with network and with sport driver.

 

Anyway, now I'm using fnord web server and I've not problems. I'm using the same site.

 

I'll do a svn update and then I'll test again with boa.

 

Regards,

 

Daniele.

TranslateQuoteReplyEditDelete

 

 

2009-05-24 09:27:52     Re: boa error

Dominik Herwald (GERMANY)

Message: 74504   

 

Hello,

 

I've got exactly the same problem with latest SVN and boa on a BF548.

 

Boa runs fine except for this stupid message.

 

There is nothing to add - the message Daniele posted looks nearly the same here.

 

Any ideas?

 

Regards,

Dominik

TranslateQuoteReplyEditDelete

 

 

2009-05-25 04:50:08     Re: boa error

Dominik Herwald (GERMANY)

Message: 74531   

 

*push*

 

For some reason this thread was not updated in the Main thread list (it's still on page 3 when I post this) with my last posting ...

Attachments

    Outcomes