2009-03-23 12:46:40     make error

Document created by Aaronwu Employee on Aug 14, 2013
Version 1Show Document
  • View in full screen mode

2009-03-23 12:46:40     make error

raghu mulagada (UNITED STATES)

Message: 71376   

 

Hello

 

I am having a problem with the make of the uClinux distribution file,

 

i get stuck at the following when i try to make it

 

 

 

make[4]: Leaving directory `/home/rkmulaga/Desktop/uClinux-dist-2008R1.5-RC3/user/boa-new/src'

make[3]: Leaving directory `/home/rkmulaga/Desktop/uClinux-dist-2008R1.5-RC3/user/boa-new'

make[2]: Leaving directory `/home/rkmulaga/Desktop/uClinux-dist-2008R1.5-RC3/user'

make[1]: *** [all] Error 2

make[1]: Leaving directory `/home/rkmulaga/Desktop/uClinux-dist-2008R1.5-RC3/user'

make: *** [subdirs] Error 1

 

 

i am using bf537 board, with vendor selection  BF537-STAMP-JFFS2

 

the kernel is linux-2.6.x

 

can anyone suggest a solution for this ?

 

Thanks

 

raghu

 

 

QuoteReplyEditDelete

 

 

2009-03-23 13:19:42     Re: make error

Robin Getz (UNITED STATES)

Message: 71377   

 

Raghu:

 

Because you are building in parrallel - that doesn't show where the error is. Try "make single" or "make NON_SMP_BUILD=1" (they are the same) - and then post the error.

 

-Robin

QuoteReplyEditDelete

 

 

2009-03-23 13:57:27     Re: make error

raghu mulagada (UNITED STATES)

Message: 71380   

 

thank you for the tip

 

i figured out the problem

 

the kernel compiled without any problem

 

thanks

 

raghu

Attachments

    Outcomes