2009-03-17 01:54:43     Bringing network up

Document created by Aaronwu Employee on Aug 14, 2013
Version 1Show Document
  • View in full screen mode

2009-03-17 01:54:43     Bringing network up

Parimala Baggiri (INDIA)

Message: 71070   

 

Hello,

 

           I am unable to pass bootargs to kernel command line. I have set bootargs as "root=/dev/mtdblock0 rw console=ttyBF0,57600 ip=192.168.4.21:192.168.4.22:192.168.4.1:255.255.255.0:bf537:eth0:off", but the same is not appearing while kernel booting.

 

It shows "Kernel Command line: " that's all no string follows that.

 

so I have to configure the network manually for each boot, that works fine. I want an automated one.

 

could you please tell where am I going wrong?

 

u-boot: U-Boot 1.1.6-svn1448 (ADI-2009R1-pre) (Mar 17 2009 - 09:51:32)

 

uClinux-dist: LiLinux version 2.6.28-rc2-ADI-2009R1-pre-svn5719

 

Regards

 

Parimala

 

 

 

 

 

 

QuoteReplyEditDelete

 

 

2009-03-17 09:07:30     Re: Bringing network up

Robin Getz (UNITED STATES)

Message: 71104   

 

Parimala:

 

Check that you have not selected CONFIG_CMDLINE_BOOL

 

-Robin

QuoteReplyEditDelete

 

 

2009-03-17 09:28:15     Re: Bringing network up

Parimala Baggiri (INDIA)

Message: 71111   

 

Hello Robin,

 

                 Yes, I have not selected that option, if I am not wrong If that option is enbled it will take the cmdline from whatever we have given for CONFIG_CMDLINE_BOOL option by ignoring the u-boot bootargs right?

 

Thank You

 

Regards

 

Parimala

QuoteReplyEditDelete

 

 

2009-03-17 09:42:57     Re: Bringing network up

Robin Getz (UNITED STATES)

Message: 71112   

 

Parimala:

 

That is correct - selecting that option will over-ride any options passed in by U-Boot.

 

The other issue is using a U-Boot and kernel that are out of sync. Are you using the same release of both?

 

-Robin

QuoteReplyEditDelete

 

 

2009-03-18 00:19:47     Re: Bringing network up

Parimala Baggiri (INDIA)

Message: 71147   

 

Hello Robin,

 

                       These are my U-boot and kernel versions from svn

 

u-boot: U-Boot 1.1.6-svn1448 (ADI-2009R1-pre) (Mar 17 2009 - 09:51:32)

 

uClinux-dist: Linux version 2.6.28-rc2-ADI-2009R1-pre-svn5719

 

Regards

 

Parimala

QuoteReplyEditDelete

 

 

2009-03-19 05:26:40     Re: Bringing network up

Parimala Baggiri (INDIA)

Message: 71261   

 

Hello,

 

           U-boot bootargs are passed correctly when I disable the option "Debug double faults" in Kernel Hacking.

 

What could be the problem?

 

Thank you

 

Regards

 

Parimala

QuoteReplyEditDelete

 

 

2009-03-20 22:07:37     Re: Bringing network up

Robin Getz (UNITED STATES)

Message: 71325   

 

Parimala:

 

I will have a look - and check it out.

 

-Robin

Attachments

    Outcomes