2009-03-11 01:26:36     adding new field to event subsystem

Document created by Aaronwu Employee on Aug 14, 2013
Version 1Show Document
  • View in full screen mode

2009-03-11 01:26:36     adding new field to event subsystem

abhrajit datta (INDIA)

Message: 70735   

 

Hi,

 

I want to add a new event type to the input subsystem. My accelerometer reports events such as tap and activity, for which there are no suitable fields in the input subsystem. Can i customize the input.c file. In which files should i have to add code if i want to do something similiar?

 

Thanks

 

Abhri

QuoteReplyEditDelete

 

 

2009-03-11 04:03:36     Re: adding new field to event subsystem

Mike Frysinger (UNITED STATES)

Message: 70738   

 

you should send your question to linux-input@vger.kernel.org as they should know ...

Attachments

    Outcomes