2009-03-04 02:41:44     how to build and run the linphone with the source-code?

Document created by Aaronwu Employee on Aug 14, 2013
Version 1Show Document
  • View in full screen mode

2009-03-04 02:41:44     how to build and run the linphone with the source-code?

wenchao zhou (CHINA)

Message: 70328   

 

Dear engineer:

 

     i  want to do some development open the souce code which has  transplanted linphone. i download the uClinux-dist-2007R1-RC3.tar.bz2 from your website  blackfin.uclinux.org/gf/project/uclinux-dist/frs/?action=FrsReleaseView&release_id=49.   i use the ADI BF533 Board and my develop enviroment is cygwin. is the souce_code right for me if i want to build the code and run the linphone on my board?

 

    i   uccompressed the uClinux-dist-2007R1-RC3.tar.bz2 packet use the command:   tar -jxvf  uClinux-dist-2007R1-RC3.tar.bz2 ,  but at last it response "tar:Error exit deleyed from previous erros",what can i do to deal with the problem?

 

   The last question is:  If i have uncompressed the packet successful it will bring a folder uClinux-dist,  what should i doif i want to build it in my cygwin enviroment?  My main destination is to build the linphone and run it on my ADI BF533 board.There is no exosip code in the folder linphone3.0 ,should i download the exosip from other website and add it into the folder  linphone3.0.   The process seems to be very difficile for  me to bulid the linphone successfully ,could you please tell me the detailed procedure?Thank you  for your help sincerely!

 

 

 

 

QuoteReplyEditDelete

 

 

2009-03-04 02:48:20     Re: how to build and run the linphone with the source-code?

Mike Frysinger (UNITED STATES)

Message: 70331   

 

cygwin isnt supported.  use real Linux.

QuoteReplyEditDelete

 

 

2009-03-04 04:02:44     Re: how to build and run the linphone with the source-code?

wenchao zhou (CHINA)

Message: 70345   

 

Hi Mike,

 

Thanks very much for you reply!

 

if i want to build the linphone or the whole source code,which edition should i use? Can i use redhat 9.0 or redhat enterprise?

 

And can you give me some suggestion about the toolchain i should use ?

 

Thanks for your help!

 

Regards

 

Zhou

QuoteReplyEditDelete

 

 

2009-03-04 04:06:57     Re: how to build and run the linphone with the source-code?

Mike Frysinger (UNITED STATES)

Message: 70346   

 

any recent distribution should work fine.  if you want to continue using Windows, you could also look at coLinux.

 

as for the toolchain, please read the documentation:

docs.blackfin.uclinux.org/doku.php?id=toolchain:installing

QuoteReplyEditDelete

 

 

2009-03-04 05:09:36     Re: how to build and run the linphone with the source-code?

wenchao zhou (CHINA)

Message: 70365   

 

Hi Mike,

 

Why did you say the cygwin environment is not supported?

 

Thanks for your help!

 

Regards

 

Zhou

QuoteReplyEditDelete

 

 

2009-03-04 13:37:30     Re: how to build and run the linphone with the source-code?

Mike Frysinger (UNITED STATES)

Message: 70376   

 

please read the faq:

docs.blackfin.uclinux.org/doku.php?id=faq

QuoteReplyEditDelete

 

 

2009-03-05 03:21:07     Re: how to build and run the linphone with the source-code?

wenchao zhou (CHINA)

Message: 70416   

 

OK,thanks for Mike's kind help.

Attachments

    Outcomes