2009-02-23 15:55:36     bluetechnix cm-bf561v2 linux booting problems

Document created by Aaronwu Employee on Aug 14, 2013
Version 1Show Document
  • View in full screen mode

2009-02-23 15:55:36     bluetechnix cm-bf561v2 linux booting problems

Alexander Heiland (GERMANY)

Message: 69770   

 

Hi,

 

I compiled a new kernel for the Bluetechnix cm-bf561v2. I used all defaults, but when I try to boot the kernel I get the following:

 

CPU:   ADSP BF561 Rev.: 0.14

Board: Bluetechnix CM-BF561v2 core module

       Support: http://www.bluetechnix.at/

Clock: VCO: 550 MHz, Core: 550 MHz, System: 110 MHz

SDRAM: 64 MB

Device ID of the Flash is 89881a

Memory Map for the Flash

0x20000000 - 0x20800000 Single Flash Chip

Please type command flinfo for information on Sectors

FLASH:   8 MB

In:    serial

Out:   serial

Err:   serial

ERROR: Can't find SMC91111 at address 28000300

Hit any key to stop autoboot:  0

CM-BF561v2> version

 

U-Boot-1.1.3-ADI-R06R2 (Jul  1 2008 - 20:10:33)

 

CM-BF561v2> loadb

## Ready for binary (kermit) download to 0x01000000 at 115200 bps...

U-Boot-1.1.3-ADI-R06R2 (Jul  1 2008 - 20:10:33)

 

CPU:   ADSP BF561 Rev.: 0.14

Board: Bluetechnix CM-BF561v2 core module

       Support: http://www.bluetechnix.at/

Clock: VCO: 550 MHz, Core: 550 MHz, System: 110 MHz

SDRAM: 64 MB

Device ID of the Flash is 89881a

Memory Map for the Flash

0x20000000 - 0x20800000 Single Flash Chip

Please type command flinfo for information on Sectors

FLASH:   8 MB

In:    serial

Out:   serial

Err:   serial

ERROR: Can't find SMC91111 at address 28000300

Hit any key to stop autoboot:  0

CM-BF561v2> version

 

U-Boot-1.1.3-ADI-R06R2 (Jul  1 2008 - 20:10:33)

 

CM-BF561v2> loadb

## Ready for binary (kermit) download to 0x01000000 at 115200 bps...

 

CM-BF561v2> bootm 1000000

## Booting image at 01000000 ...

   Image Name:   uClinux Kernel and ext2

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    2078168 Bytes =  2 MB

   Load Address: 00001000

   Entry Point:  00144000

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 144000

����f~f����f�����x��x�x�������`��憘f�f�����~����f�����ff�����~�x��

 

 

Can anyone help me with this?

 

Best regards,

 

Alexander

 

 

 

config_kernel

TranslateQuoteReplyEditDelete

 

 

2009-02-23 16:04:49     Re: bluetechnix cm-bf561v2 linux booting problems

Mike Frysinger (UNITED STATES)

Message: 69771   

 

most likely you didnt set the serial baud properly, so u-boot runs at 115200 but linux runs at 57600

 

also, that version of u-boot isnt supported here ... you should upgrade to 2008R1.5

QuoteReplyEditDelete

 

 

2009-02-25 16:52:42     Re: bluetechnix cm-bf561v2 linux booting problems

Alexander Heiland (GERMANY)

Message: 69915   

 

thank you very much for your help.

Attachments

Outcomes