2009-02-19 11:06:34     svn uClinux-dist 2009 pre and Unable to mount root fs

Document created by Aaronwu Employee on Aug 13, 2013
Version 1Show Document
  • View in full screen mode

2009-02-19 11:06:34     svn uClinux-dist 2009 pre and Unable to mount root fs

Daniele Pagani (ITALY)

Message: 69643   

 

Dear sirs,

 

I've done:

 

1) download

 

snaps 3 - Alpha uImage-SVN-r7745-bf537-stamp 4.46 Mb

 

2) load uImage by u-boot on my bf537 Stamp

 

3) bootm 0x1000000

 

4) all works fine

 

Then, I've done:

 

1) done all steps in order to use "live" distributions

 

2) make with default settings (after selected the BF537 Stamp board) (no compilation error)

 

3) uclinux svn revision 7741, linux-kernel revision 6101, toolchain revision 3185, u-boot 1676 (but I use the same u-boot on the same board)

 

4) then, I load by u-boot uImage.initramfs I've as follows:

 

...           

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 95

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, m

dc_clk=2500000Hz(mdc_div=19)@sclk=100MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_b

ase@ffc00500, dma channel@7

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-01-01 00:00:01 UTC (1)

List of all partitions:

No filesystem could mount root, tried:

Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)

 

Any idea?

 

Best regards,

 

Daniele.

 

 

 

 

TranslateQuoteReplyEditDelete

 

 

2009-02-19 12:38:55     Re: svn uClinux-dist 2009 pre and Unable to mount root fs

Mike Frysinger (UNITED STATES)

Message: 69646   

 

run `make distclean` then `make AnalogDevices/BF537-STAMP_default`

 

then load the file named "uImage"

Attachments

    Outcomes