2009-02-18 11:25:02     How Do I Automount a USB FLASH Drive

Document created by Aaronwu Employee on Aug 13, 2013
Version 1Show Document
  • View in full screen mode

2009-02-18 11:25:02     How Do I Automount a USB FLASH Drive

David Kasper (UNITED STATES)

Message: 69571   

 

I have the STAMP USB add-on card working with the BF-537.  I can mount a USB FLASH drive and see the files.  The kernel also detects when the drive is inserted and removed.  Is there a way to have the kernel automatically mount the drive when inserted?  Also, what is the best way for a user application to detect when the drive is inserted or removed?

 

Thanks,

 

David Kasper

QuoteReplyEditDelete

 

 

2009-02-18 11:59:31     Re: How Do I Automount a USB FLASH Drive

Robin Getz (UNITED STATES)

Message: 69577   

 

David:

 

Have a look at the hotplug docs:

 

docs.blackfin.uclinux.org/doku.php?id=linux-kernel:hotplug

 

-Robin

Attachments

    Outcomes